AN11755 - Fig 44 and Fig 51 incomplete

cancel
Showing results for 
Search instead for 
Did you mean: 

AN11755 - Fig 44 and Fig 51 incomplete

59 Views
Contributor I

I am writing regarding the doc AN11755 Antenna design guide of PN7150 https://www.nxp.com/docs/en/application-note/AN11755.pdf 

Some figures are incomplete, e.g. Fig 44 and Fig 51. Is there an updated version?

Regards

Ahmed

Labels (1)
Tags (3)
0 Kudos
1 Reply

2 Views
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, There is not the updated version for it so far. the version 1.7 is the latest version.  Thanks for your understanding. 

Have a  nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos