66301 Chip question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

66301 Chip question

2,821 Views
eric4
Contributor I

I am looking to understand exactly what chip this is and if it is the same class as the CLRC633.  What are the differences?

0 Kudos
Reply
1 Reply

2,751 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Eric,

Yes, it is also CLRC663, but not plus version, the plus is CLRC66303,  and it provides the following features comparing with CLRC663:

--Provides larger temperature range.
--Provides higher ITVDD range.
--Provides improved LPCD.

and they are pin to pin compatible.

Hope that makes sense,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply