請教各位MFRC630 Reader的Code size大小
能否用在LPC804 MCU上?
Hi,
Hope you are doing well. The Basic Discovery Loop example of the Reader Library provided by NXP (CLRC663), after the compilation process, shows a used size of the flash of approximately 113,404 Bytes. The MFRC630 is a derivative product of the CLRC663, so it is almost the same size.
Still, consider that the LPC804 has up to 32 KB on-chip EEPROM based flash programming memory, so the size might not be enough for your application,
Best Regards,
Ricardo