关于PN532挂起功能问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

关于PN532挂起功能问题

750件の閲覧回数
zsj
Contributor I

您好,我在一个方案中选择PN532,解决了读写卡的问题,现在想读一张卡后,只有卡离开后才能再读取。就是挂起/中止PN532的意思,当卡再次进入射频场,可以自动从挂起/中止中退出,可以实现吗?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

643件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Zhao,

Would you please confirm if you want PN532 into HALT mode when the card  is in the field at the first time and then wake up the device when the card approach the device at the second time?  Would you please help to clarify? Thanks for your patience!

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

643件の閲覧回数
zsj
Contributor I

做过的朋友加个QQ交流下奥  1530908765

0 件の賞賛
返信