i.MX6ULL EVK running Yocto Linux + PN7160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL EVK running Yocto Linux + PN7160

i.MX6ULL EVK running Yocto Linux + PN7160

Hardware:

1. i.MX6ULL EVK board

pic1.jfif

 

2. OM27160A1HN

pic2.jfif

 

Software:

1. Build the Yocto Linux BSP for i.MX6ULL EVK.

Here are the steps:

$ mkdir L6.6.36_2.1.0
$ cd L6.6.36_2.1.0
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml
$ repo sync

 

$ DISTRO=fsl-imx-xwayland MACHINE=imx6ull14x14evk source imx-setup-release.sh -b build-for-6ullevk
$ bitbake core-image-full-cmdline

 

2. Add the nxpnfc driver to kernel

After the BSP build succeed, the kernel source code is located here:

L6.6.36_2.1.0/build-for-6ullevk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/6.6.36+git/git/

 

Clone the nxpnfc repository into the kernel directory, replacing existing implementation:

$ cd L6.6.36_2.1.0/build-for-6ullevk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/6.6.36+git/git/
$ rm -rf drivers/nfc
$ git clone https://github.com/NXPNFCLinux/nxpnfc.git drivers/nfc 

 This will end-up with the folder drivers/nfc containing the following files:

• README.md: repository information
• Makefile: driver heading makefile
• Kconfig: driver configuration file
• LICENSE: driver licensing terms

• i2c_devicetree.txt: example of I²C device tree definition
• spi_devicetree.txt: example of SPI device tree definition
• nfc sub folder containing:
– Makefile:
– common.c: generic driver implementation
– common.h: generic driver interface definition
– i2c.c: I2C specific driver implementation
– i2c.h: I2C specific driver interface definition
– spi.c: SPI-specific driver implementation
– spi.h: SPI-specific driver interface definition

 

Through kernel menuconfig procedure include the targeted driver to the build, as built-in (<*>):

$ bitbake linux-imx -c menuconfig

<*> NFC I2C Slave driver for NXP-NFCC

 

kernel_menuconfig.png

 

 

3. Connection between i.MX6ULL EVK and the PN7160

There are some pins on the Arduino header on the i.MX6ULL EVK board can be used to connect the PN7160 board. Below is the schematic of the Arduino headers on the i.MX6ULL EVK board. The two I2C2 pins can be used for I2C connection. The UART2_RX, UART2_TX and UART2_RTS can be changed to GPIO for connecting IRQ, VEN and DWL_REQ of PN7160, respectively.

arduino_header_6ullevk.png

Below is the J1704 and J1703 on the EVK board.

pic3.jfif

 

Below is the schematic of Arduino interface on OM27160A1HN.

om27160_arduino.png

There is a connector board (OM29110ARD-B). The OM27160A1HN is connecting on top of it. Below is the connectors board schematic.

47957.png

So, on the i.MX6ULL EVK board, we need I2C2 SDA and I2C2 SCL for I2C connections. And 3 GPIO pins for PN7160's IRQ, VEN and DWL_REQ.

Here is the connection between i.MX6ULL EVK and OM29110ARD-B.

OM29110ARD-B pin i.MX6ULL EVK pin
I2C_SCL J2-1 I2C2_SCL J1704-10
I2C_SDA J2-2 I2C2_SDA J1704-9
GPIO_0 J2-10 GPIO1_21 J1703-1
GPIO_1 J4_1 GPIO1_20 J1703-2
GPIO_2 J4_2 GPIO1_25 J1703-3
3.3V J1-4 3.3V J1705-4
5V J1-5 5V J1705-5
GND J1-6 GND J1705-6

 

 

 4. Modify the device tree file of i.MX6ull evk.

The device tree file for i.MX6ULL evk is imx6ul-14x14-evk.dtsi. The location of the device tree file is here:

L6.6.36_2.1.0/build-for-6ullevk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/6.6.36+git/git/arch/arm/boot/dts/nxp/imx/imx6ul-14x14-evk.dtsi

 

As we don't use the UART2, we disabled it.

&uart2 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_uart2>;
	uart-has-rtscts;
	/* for DTE mode, add below change */
	/* fsl,dte-mode; */
	/* pinctrl-0 = <&pinctrl_uart2dte>; */
	status = "disabled";  // <--- change the status to "disabled"

	bluetooth {
		compatible = "nxp,88w8987-bt";
	};
};

 

Put the below nxpnfc under the &I2C2 node.

nxpnfc: nxpnfc@28 {
		compatible = "nxp,nxpnfc";
		reg = <0x28>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_nfcgpio>;
		nxp,nxpnfc-irq = <&gpio1 21 0>;
		nxp,nxpnfc-ven = <&gpio1 20 0>;
		nxp,nxpnfc-fw-dwnld = <&gpio1 25 0>;
	};

 

Like this:

under_I2C2_in_dts.png

Add the gpios for nxpnfc.

	pinctrl_nfcgpio: nfcgpiogrp {
		fsl,pins = <
			MX6UL_PAD_UART2_RX_DATA__GPIO1_IO21   0xb0  //irq
			MX6UL_PAD_UART2_TX_DATA__GPIO1_IO20   0xb0  //ven
			MX6UL_PAD_UART3_RX_DATA__GPIO1_IO25   0xb0  //dwld req
		>;
	};

 

 

5. Re-compile the kernel and the whole image.

$ bitbake linux-imx -c compile
$ bitbake core-image-full-cmdline

 

 

6. Using UUU to program the image to the board.

The built image is .wic.zst file. We need to program it to the board. It is located in the deploy folder below.

L6.6.36_2.1.0/build-for-6ullevk/tmp/deploy/images/imx6ull14x14evk/core-image-full-cmdline-imx6ull14x14evk.rootfs-20241113103828.wic.zst

 

Download the UUU.exe from here:

https://github.com/nxp-imx/mfgtools/releases

 

Download the Demo image for i.MX6ULL EVK from the Linux BSP web page.

linux_bsp_web_page.png

 

Unzip the demo image file to a folder. And then copy the UUU.exe to the same demo image folder.

 

Connect the board to your PC using the USB cable. Switch the boot mode to "Serial Downloader mode"

uuu_download.jfif

 

On the PC side, run the below command to program the image to SD card on the i.MX6ULL EVK.

uuu -b sd_all core-image-full-cmdline-imx6ull14x14evk.rootfs-20241112083235.wic.zst

 

Then switch the boot mode to "Internal Boot (Development)". Restart the board.

Now, you can login as "root" and use the board.

login_root.png

And you can see the nxpnfc driver is properly loaded.

dmesg_dev.png

 

 

7. Build the NFC Library and the nfcDemoApp in Yocto

    $ git clone https://github.com/NXPNFCLinux/meta-nxp-nfc.git 

Then, the NFC library recipe is located in L6.6.36_2.1.0/sources/meta-nxp-nfc/recipes-nfc/nxp_nfc. Change the recipe nxp-nfc_git.bb as below:

# Copyright (C) 2016 NXP Semiconductors

DESCRIPTION = "Linux NFC stack for NCI based NXP NFC Controllers."
LICENSE = "Apache-2.0"
LIC_FILES_CHKSUM = "file://LICENSE.txt;md5=86d3f3a95c324c9479bd8986968f4327"

SRC_URI = " \
    git://github.com/NXPNFCLinux/linux_libnfc-nci.git;branch=NCI2.0_PN7160;protocol=https \
"
SRCREV = "6bf9f42b94e267f6384043009bda84c11e7ebbaa"
SRC_URI[sha256sum] = "47bdc27108fc8d66ce5d6c33f76b419cdef20c24b9e187ada8e689d1bd7f79c7"

inherit autotools pkgconfig lib_package

S = "${WORKDIR}/git"

 

  • Add the meta-nxp-nfc layer to the build definition. Updating file build_dir/conf/bblayers.conf with:

BBLAYERS += " ${BSPDIR}/sources/meta-nxp-nfc"

 

  • Build meta-nxp-nfc layer:

    $ bitbake nxp-nfc

After build succeed, the library files and the nfcDemoApp are located in here :

L6.6.36_2.1.0/build-for-6ullevk/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/nxp-nfc/git/

 

Use the "scp" command to copy the files to the EVK board via the Network. If the folder is not exist on the EVK, please use "mkdir" to make the folder on the EVK first. Then use the "scp" command. 

Here is the example: (**The IP address below should change to your EVK's IP address.)

scp build/.libs/* root@10.192.246.136:/.libs/

scp_command.png

scp image/etc/libnfc* root@10.192.246.136:/etc/

 scp_command2.png

scp image/usr/lib/* root@10.192.246.136:/usr/lib

 scp_command3.png

 

On the EVK board:

root@imx6ull14x14evk:/# mkdir /usr/local
root@imx6ull14x14evk:/# mkdir /usr/local/etc
root@imx6ull14x14evk:/# cp /etc/libnfc-nci.conf /usr/local/etc

 

Now, you can run the nfcDemoApp on the i.MX6ULL EVK.

root@imx6ull14x14evk:/# cd .libs/
root@imx6ull14x14evk:/.libs# ./nfcDemoApp poll

nfcDemoApp.png

 

 

 

References:

1. i.MX Yocto Project User's guide

2. PN7160 Linux Porting Guide

3. MCIMX6ULL-EVK_DESIGNFILES

4. OM27160A1HN Hardware Design Files

5. OM29110 NFC’s SBC Interface Board Design Files

6. PN7150 NFC Controller on i.MX8M mini evk running Yocto

Labels (1)
%3CLINGO-SUB%20id%3D%22lingo-sub-1994337%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Ei.MX6ULL%20EVK%20running%20Yocto%20Linux%20%2B%20PN7160%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1994337%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%0A%3CP%3E%3CSTRONG%3EHardware%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E1.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdesign-center%2Fdevelopment-boards-and-designs%2Fi-mx-evaluation-and-development-boards%2Fevaluation-kit-for-the-i-mx-6ull-and-6ulz-applications-processor%3AMCIMX6ULL-EVK%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ei.MX6ULL%20EVK%20board%20%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22pic1.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pic1.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310467i33B00D038AAF0D81%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pic1.jfif%22%20alt%3D%22pic1.jfif%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E2.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fproducts%2Frfid-nfc%2Fnfc-hf%2Fnfc-readers%2Fom27160-development-kits-for-pn7160-plugn-play-nfc-controller%3APN7160-EVK%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EOM27160A1HN%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22pic2.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pic2.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310468i037466CD4976AA6F%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pic2.jfif%22%20alt%3D%22pic2.jfif%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3ESoftware%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3E1.%20Build%20the%20Yocto%20Linux%20BSP%20for%20i.MX6ULL%20EVK.%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3EHere%20are%20the%20steps%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%24%20mkdir%20L6.6.36_2.1.0%0A%24%20cd%20L6.6.36_2.1.0%0A%24%20repo%20init%20-u%20https%3A%2F%2Fgithub.com%2Fnxp-imx%2Fimx-manifest%20-b%20imx-linux-scarthgap%20-m%20imx-6.6.36-2.1.0.xml%0A%24%20repo%20sync%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%24%20DISTRO%3Dfsl-imx-xwayland%20MACHINE%3Dimx6ull14x14evk%20source%20imx-setup-release.sh%20-b%20build-for-6ullevk%0A%24%20bitbake%20core-image-full-cmdline%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E2.%20Add%20the%20nxpnfc%20driver%20to%20kernel%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3EAfter%20the%20BSP%20build%20succeed%2C%20the%20kernel%20source%20code%20is%20located%20here%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3EL6.6.36_2.1.0%2Fbuild-for-6ullevk%2Ftmp%2Fwork%2Fimx6ull14x14evk-poky-linux-gnueabi%2Flinux-imx%2F6.6.36%2Bgit%2Fgit%2F%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EClone%20the%20nxpnfc%20repository%20into%20the%20kernel%20directory%2C%20replacing%20existing%20implementation%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%24%20cd%20L6.6.36_2.1.0%2Fbuild-for-6ullevk%2Ftmp%2Fwork%2Fimx6ull14x14evk-poky-linux-gnueabi%2Flinux-imx%2F6.6.36%2Bgit%2Fgit%2F%0A%24%20rm%20-rf%20drivers%2Fnfc%0A%24%20git%20clone%20https%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fnxpnfc.git%20drivers%2Fnfc%20%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CP%3E%26nbsp%3BThis%20will%20end-up%20with%20the%20folder%20drivers%2Fnfc%20containing%20the%20following%20files%3A%3C%2FP%3E%0A%3CP%3E%E2%80%A2%20README.md%3A%20repository%20information%3CBR%20%2F%3E%E2%80%A2%20Makefile%3A%20driver%20heading%20makefile%3CBR%20%2F%3E%E2%80%A2%20Kconfig%3A%20driver%20configuration%20file%3CBR%20%2F%3E%E2%80%A2%20LICENSE%3A%20driver%20licensing%20terms%3C%2FP%3E%0A%3CP%3E%E2%80%A2%20i2c_devicetree.txt%3A%20example%20of%20I%C2%B2C%20device%20tree%20definition%3CBR%20%2F%3E%E2%80%A2%20spi_devicetree.txt%3A%20example%20of%20SPI%20device%20tree%20definition%3CBR%20%2F%3E%E2%80%A2%20nfc%20sub%20folder%20containing%3A%3CBR%20%2F%3E%E2%80%93%20Makefile%3A%3CBR%20%2F%3E%E2%80%93%20common.c%3A%20generic%20driver%20implementation%3CBR%20%2F%3E%E2%80%93%20common.h%3A%20generic%20driver%20interface%20definition%3CBR%20%2F%3E%E2%80%93%20i2c.c%3A%20I2C%20specific%20driver%20implementation%3CBR%20%2F%3E%E2%80%93%20i2c.h%3A%20I2C%20specific%20driver%20interface%20definition%3CBR%20%2F%3E%E2%80%93%20spi.c%3A%20SPI-specific%20driver%20implementation%3CBR%20%2F%3E%E2%80%93%20spi.h%3A%20SPI-specific%20driver%20interface%20definition%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EThrough%20kernel%20menuconfig%20procedure%20include%20the%20targeted%20driver%20to%20the%20build%2C%20as%20built-in%20(%26lt%3B*%26gt%3B)%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%24%20bitbake%20linux-imx%20-c%20menuconfig%0A%0A%26lt%3B*%26gt%3B%20NFC%20I2C%20Slave%20driver%20for%20NXP-NFCC%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22kernel_menuconfig.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22kernel_menuconfig.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310697i6F5368A4AF798E15%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22kernel_menuconfig.png%22%20alt%3D%22kernel_menuconfig.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E3.%20Connection%20between%20i.MX6ULL%20EVK%20and%20the%20PN7160%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3EThere%20are%20some%20pins%20on%20the%20Arduino%20header%20on%20the%20i.MX6ULL%20EVK%20board%20can%20be%20used%20to%20connect%20the%20PN7160%20board.%20Below%20is%20the%20schematic%20of%20the%20Arduino%20headers%20on%20the%20i.MX6ULL%20EVK%20board.%20The%20two%20I2C2%20pins%20can%20be%20used%20for%20I2C%20connection.%20The%20UART2_RX%2C%20UART2_TX%20and%20UART2_RTS%20can%20be%20changed%20to%20GPIO%20for%20connecting%20IRQ%2C%20VEN%20and%20DWL_REQ%20of%20PN7160%2C%20respectively.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22arduino_header_6ullevk.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22arduino_header_6ullevk.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310479i01E4B5001DBC1157%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22arduino_header_6ullevk.png%22%20alt%3D%22arduino_header_6ullevk.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EBelow%20is%20the%20J1704%20and%20J1703%20on%20the%20EVK%20board.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22pic3.jfif%22%20style%3D%22width%3A%20600px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pic3.jfif%22%20style%3D%22width%3A%20600px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310485i63C0C9B51A34118A%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pic3.jfif%22%20alt%3D%22pic3.jfif%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EBelow%20is%20the%20schematic%20of%20Arduino%20interface%20on%20OM27160A1HN.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22om27160_arduino.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22om27160_arduino.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310495i65503B47B08C7EE4%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22om27160_arduino.png%22%20alt%3D%22om27160_arduino.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EThere%20is%20a%20connector%20board%20(OM29110ARD-B).%20The%20OM27160A1HN%20is%20connecting%20on%20top%20of%20it.%20Below%20is%20the%20connectors%20board%20schematic.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2247957.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2247957.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310502i6926B041F81390D0%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2247957.png%22%20alt%3D%2247957.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3ESo%2C%20on%20the%20i.MX6ULL%20EVK%20board%2C%20we%20need%20I2C2%20SDA%20and%20I2C2%20SCL%20for%20I2C%20connections.%20And%203%20GPIO%20pins%20for%20PN7160's%20IRQ%2C%20VEN%20and%20DWL_REQ.%3C%2FP%3E%0A%3CP%3EHere%20is%20the%20connection%20between%20i.MX6ULL%20EVK%20and%20OM29110ARD-B.%3C%2FP%3E%0A%3CTABLE%20style%3D%22width%3A%20450px%3B%22%20width%3D%22450%22%3E%0A%3CTBODY%3E%0A%3CTR%3E%0A%3CTD%20width%3D%22118%22%3EOM29110ARD-B%3C%2FTD%3E%0A%3CTD%20width%3D%2254%22%3Epin%3C%2FTD%3E%0A%3CTD%20width%3D%22146%22%3Ei.MX6ULL%20EVK%3C%2FTD%3E%0A%3CTD%20width%3D%2271%22%3Epin%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EI2C_SCL%3C%2FTD%3E%0A%3CTD%3EJ2-1%3C%2FTD%3E%0A%3CTD%3EI2C2_SCL%3C%2FTD%3E%0A%3CTD%3EJ1704-10%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EI2C_SDA%3C%2FTD%3E%0A%3CTD%3EJ2-2%3C%2FTD%3E%0A%3CTD%3EI2C2_SDA%3C%2FTD%3E%0A%3CTD%3EJ1704-9%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EGPIO_0%3C%2FTD%3E%0A%3CTD%3EJ2-10%3C%2FTD%3E%0A%3CTD%3EGPIO1_21%3C%2FTD%3E%0A%3CTD%3EJ1703-1%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EGPIO_1%3C%2FTD%3E%0A%3CTD%3EJ4_1%3C%2FTD%3E%0A%3CTD%3EGPIO1_20%3C%2FTD%3E%0A%3CTD%3EJ1703-2%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EGPIO_2%3C%2FTD%3E%0A%3CTD%3EJ4_2%3C%2FTD%3E%0A%3CTD%3EGPIO1_25%3C%2FTD%3E%0A%3CTD%3EJ1703-3%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3E3.3V%3C%2FTD%3E%0A%3CTD%3EJ1-4%3C%2FTD%3E%0A%3CTD%3E3.3V%3C%2FTD%3E%0A%3CTD%3EJ1705-4%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3E5V%3C%2FTD%3E%0A%3CTD%3EJ1-5%3C%2FTD%3E%0A%3CTD%3E5V%3C%2FTD%3E%0A%3CTD%3EJ1705-5%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%3EGND%3C%2FTD%3E%0A%3CTD%3EJ1-6%3C%2FTD%3E%0A%3CTD%3EGND%3C%2FTD%3E%0A%3CTD%3EJ1705-6%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3C%2FTBODY%3E%0A%3C%2FTABLE%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E%26nbsp%3B4.%20Modify%20the%20device%20tree%20file%20of%20i.MX6ull%20evk.%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3EThe%20device%20tree%20file%20for%20i.MX6ULL%20evk%20is%20imx6ul-14x14-evk.dtsi.%20The%20location%20of%20the%20device%20tree%20file%20is%20here%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3EL6.6.36_2.1.0%2Fbuild-for-6ullevk%2Ftmp%2Fwork%2Fimx6ull14x14evk-poky-linux-gnueabi%2Flinux-imx%2F6.6.36%2Bgit%2Fgit%2Farch%2Farm%2Fboot%2Fdts%2Fnxp%2Fimx%2Fimx6ul-14x14-evk.dtsi%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EAs%20we%20don't%20use%20the%20UART2%2C%20we%20disabled%20it.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%26amp%3Buart2%20%7B%0A%09pinctrl-names%20%3D%20%22default%22%3B%0A%09pinctrl-0%20%3D%20%26lt%3B%26amp%3Bpinctrl_uart2%26gt%3B%3B%0A%09uart-has-rtscts%3B%0A%09%2F*%20for%20DTE%20mode%2C%20add%20below%20change%20*%2F%0A%09%2F*%20fsl%2Cdte-mode%3B%20*%2F%0A%09%2F*%20pinctrl-0%20%3D%20%26lt%3B%26amp%3Bpinctrl_uart2dte%26gt%3B%3B%20*%2F%0A%09status%20%3D%20%22disabled%22%3B%20%20%2F%2F%20%26lt%3B---%20change%20the%20status%20to%20%22disabled%22%0A%0A%09bluetooth%20%7B%0A%09%09compatible%20%3D%20%22nxp%2C88w8987-bt%22%3B%0A%09%7D%3B%0A%7D%3B%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EPut%20the%20below%20nxpnfc%20under%20the%20%26amp%3BI2C2%20node.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Enxpnfc%3A%20nxpnfc%4028%20%7B%0A%09%09compatible%20%3D%20%22nxp%2Cnxpnfc%22%3B%0A%09%09reg%20%3D%20%26lt%3B0x28%26gt%3B%3B%0A%09%09pinctrl-names%20%3D%20%22default%22%3B%0A%09%09pinctrl-0%20%3D%20%26lt%3B%26amp%3Bpinctrl_nfcgpio%26gt%3B%3B%0A%09%09nxp%2Cnxpnfc-irq%20%3D%20%26lt%3B%26amp%3Bgpio1%2021%200%26gt%3B%3B%0A%09%09nxp%2Cnxpnfc-ven%20%3D%20%26lt%3B%26amp%3Bgpio1%2020%200%26gt%3B%3B%0A%09%09nxp%2Cnxpnfc-fw-dwnld%20%3D%20%26lt%3B%26amp%3Bgpio1%2025%200%26gt%3B%3B%0A%09%7D%3B%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3ELike%20this%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22under_I2C2_in_dts.png%22%20style%3D%22width%3A%20602px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22under_I2C2_in_dts.png%22%20style%3D%22width%3A%20602px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312555iF9CFED6DDA5F7328%2Fimage-dimensions%2F602x544%3Fv%3Dv2%22%20width%3D%22602%22%20height%3D%22544%22%20role%3D%22button%22%20title%3D%22under_I2C2_in_dts.png%22%20alt%3D%22under_I2C2_in_dts.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EAdd%20the%20gpios%20for%20nxpnfc.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%09pinctrl_nfcgpio%3A%20nfcgpiogrp%20%7B%0A%09%09fsl%2Cpins%20%3D%20%26lt%3B%0A%09%09%09MX6UL_PAD_UART2_RX_DATA__GPIO1_IO21%20%20%200xb0%20%20%2F%2Firq%0A%09%09%09MX6UL_PAD_UART2_TX_DATA__GPIO1_IO20%20%20%200xb0%20%20%2F%2Fven%0A%09%09%09MX6UL_PAD_UART3_RX_DATA__GPIO1_IO25%20%20%200xb0%20%20%2F%2Fdwld%20req%0A%09%09%26gt%3B%3B%0A%09%7D%3B%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E5.%20Re-compile%20the%20kernel%20and%20the%20whole%20image.%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%24%20bitbake%20linux-imx%20-c%20compile%0A%24%20bitbake%20core-image-full-cmdline%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E6.%20Using%20UUU%20to%20program%20the%20image%20to%20the%20board.%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3EThe%20built%20image%20is%20.wic.zst%20file.%20We%20need%20to%20program%20it%20to%20the%20board.%20It%20is%20located%20in%20the%20deploy%20folder%20below.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3EL6.6.36_2.1.0%2Fbuild-for-6ullevk%2Ftmp%2Fdeploy%2Fimages%2Fimx6ull14x14evk%2Fcore-image-full-cmdline-imx6ull14x14evk.rootfs-20241113103828.wic.zst%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EDownload%20the%20UUU.exe%20from%20here%3A%3C%2FP%3E%0A%3CP%3E%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fnxp-imx%2Fmfgtools%2Freleases%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Ehttps%3A%2F%2Fgithub.com%2Fnxp-imx%2Fmfgtools%2Freleases%3C%2FA%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EDownload%20the%20Demo%20image%20for%20i.MX6ULL%20EVK%20from%20the%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fembedded-software%2Fi-mx-software%2Fembedded-linux-for-i-mx-applications-processors%3AIMXLINUX%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3ELinux%20BSP%20web%20page%3C%2FA%3E.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22linux_bsp_web_page.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22linux_bsp_web_page.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F310537iEB6D000047C9F78D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22linux_bsp_web_page.png%22%20alt%3D%22linux_bsp_web_page.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EUnzip%20the%20demo%20image%20file%20to%20a%20folder.%20And%20then%20copy%20the%20UUU.exe%20to%20the%20same%20demo%20image%20folder.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EConnect%20the%20board%20to%20your%20PC%20using%20the%20USB%20cable.%20Switch%20the%20boot%20mode%20to%20%22Serial%20Downloader%20mode%22%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22uuu_download.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22uuu_download.jfif%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312557i8A109B3D317573CA%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22uuu_download.jfif%22%20alt%3D%22uuu_download.jfif%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EOn%20the%20PC%20side%2C%20run%20the%20below%20command%20to%20program%20the%20image%20to%20SD%20card%20on%20the%20i.MX6ULL%20EVK.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Euuu%20-b%20sd_all%20core-image-full-cmdline-imx6ull14x14evk.rootfs-20241112083235.wic.zst%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EThen%20switch%20the%20boot%20mode%20to%20%22Internal%20Boot%20(Development)%22.%20Restart%20the%20board.%3C%2FP%3E%0A%3CP%3ENow%2C%20you%20can%20login%20as%20%22root%22%20and%20use%20the%20board.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22login_root.png%22%20style%3D%22width%3A%20873px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22login_root.png%22%20style%3D%22width%3A%20873px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312559i632ACDC26E84E575%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22login_root.png%22%20alt%3D%22login_root.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EAnd%20you%20can%20see%20the%20nxpnfc%20driver%20is%20properly%20loaded.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22dmesg_dev.png%22%20style%3D%22width%3A%20920px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22dmesg_dev.png%22%20style%3D%22width%3A%20920px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312561i8E7EBDDB5F0BAEDE%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22dmesg_dev.png%22%20alt%3D%22dmesg_dev.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3E%3CSTRONG%3E7.%20Build%20the%20NFC%20Library%20and%20the%20nfcDemoApp%20in%20Yocto%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CDIV%20class%3D%22%22%3E%0A%3CUL%3E%0A%3CLI%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3EIn%20the%20Yocto's%20%3CSPAN%3Esources%3C%2FSPAN%3E%20directory%2C%20download%20the%20meta-nxp-nfc%20layer%20from%20%3CA%20class%3D%22link-titled%22%20title%3D%22https%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc%22%20href%3D%22https%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ehttps%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc%3C%2FA%3E%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3C%2FDIV%3E%0A%3CBLOCKQUOTE%20class%3D%22jive_macro_quote%20jive-quote%20jive_text_macro%22%3E%0A%3CP%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%24%20git%20clone%20%3CA%20class%3D%22link-titled%22%20title%3D%22https%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc.git%22%20href%3D%22https%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc.git%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ehttps%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Fmeta-nxp-nfc.git%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3C%2FBLOCKQUOTE%3E%0A%3CP%3EThen%2C%20the%20NFC%20library%20recipe%20is%20located%20in%20L6.6.36_2.1.0%2Fsources%2Fmeta-nxp-nfc%2Frecipes-nfc%2Fnxp_nfc.%20Change%20the%20recipe%20nxp-nfc_git.bb%20as%20below%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%23%20Copyright%20(C)%202016%20NXP%20Semiconductors%0A%0ADESCRIPTION%20%3D%20%22Linux%20NFC%20stack%20for%20NCI%20based%20NXP%20NFC%20Controllers.%22%0ALICENSE%20%3D%20%22Apache-2.0%22%0ALIC_FILES_CHKSUM%20%3D%20%22file%3A%2F%2FLICENSE.txt%3Bmd5%3D86d3f3a95c324c9479bd8986968f4327%22%0A%0ASRC_URI%20%3D%20%22%20%5C%0A%20%20%20%20git%3A%2F%2Fgithub.com%2FNXPNFCLinux%2Flinux_libnfc-nci.git%3Bbranch%3DNCI2.0_PN7160%3Bprotocol%3Dhttps%20%5C%0A%22%0ASRCREV%20%3D%20%226bf9f42b94e267f6384043009bda84c11e7ebbaa%22%0ASRC_URI%5Bsha256sum%5D%20%3D%20%2247bdc27108fc8d66ce5d6c33f76b419cdef20c24b9e187ada8e689d1bd7f79c7%22%0A%0Ainherit%20autotools%20pkgconfig%20lib_package%0A%0AS%20%3D%20%22%24%7BWORKDIR%7D%2Fgit%22%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CUL%3E%0A%3CLI%3EAdd%20the%20meta-nxp-nfc%20layer%20to%20the%20build%20definition.%20Updating%20file%20%3CSPAN%3Ebuild_dir%2Fconf%2Fbblayers.conf%3C%2FSPAN%3E%20with%3A%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CBLOCKQUOTE%20class%3D%22jive_macro_quote%20jive-quote%20jive_text_macro%22%3E%0A%3CP%3EBBLAYERS%20%2B%3D%20%22%20%24%7BBSPDIR%7D%2Fsources%2Fmeta-nxp-nfc%22%3C%2FP%3E%0A%3C%2FBLOCKQUOTE%3E%0A%3CBR%20%2F%3E%0A%3CUL%3E%0A%3CLI%3EBuild%20meta-nxp-nfc%20layer%3A%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CBLOCKQUOTE%20class%3D%22jive_macro_quote%20jive-quote%20jive_text_macro%22%3E%0A%3CP%3E%3CSPAN%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%24%20bitbake%20nxp-nfc%3C%2FSPAN%3E%3C%2FP%3E%0A%3C%2FBLOCKQUOTE%3E%0A%3CP%3EAfter%20build%20succeed%2C%20the%20library%20files%20and%20the%20nfcDemoApp%20are%20located%20in%20here%20%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3EL6.6.36_2.1.0%2Fbuild-for-6ullevk%2Ftmp%2Fwork%2Fcortexa7t2hf-neon-poky-linux-gnueabi%2Fnxp-nfc%2Fgit%2F%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3EUse%20the%20%22scp%22%20command%20to%20copy%20the%20files%20to%20the%20EVK%20board%20via%20the%20Network.%20If%20the%20folder%20is%20not%20exist%20on%20the%20EVK%2C%20please%20use%20%22mkdir%22%20to%20make%20the%20folder%20on%20the%20EVK%20first.%20Then%20use%20the%20%22scp%22%20command.%26nbsp%3B%3C%2FP%3E%0A%3CP%3EHere%20is%20the%20example%3A%20(**The%20IP%20address%20below%20should%20change%20to%20your%20EVK's%20IP%20address.)%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Escp%20build%2F.libs%2F*%20root%4010.192.246.136%3A%2F.libs%2F%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22scp_command.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22scp_command.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312707i7AA63C55E2908D1C%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22scp_command.png%22%20alt%3D%22scp_command.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Escp%20image%2Fetc%2Flibnfc*%20root%4010.192.246.136%3A%2Fetc%2F%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CP%3E%26nbsp%3B%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22scp_command2.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22scp_command2.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312708iAAF198AB90969F96%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22scp_command2.png%22%20alt%3D%22scp_command2.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Escp%20image%2Fusr%2Flib%2F*%20root%4010.192.246.136%3A%2Fusr%2Flib%0A%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CP%3E%26nbsp%3B%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22scp_command3.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22scp_command3.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312709i35D0BB50D1ADBA36%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22scp_command3.png%22%20alt%3D%22scp_command3.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EOn%20the%20EVK%20board%3A%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Eroot%40imx6ull14x14evk%3A%2F%23%20mkdir%20%2Fusr%2Flocal%0Aroot%40imx6ull14x14evk%3A%2F%23%20mkdir%20%2Fusr%2Flocal%2Fetc%0Aroot%40imx6ull14x14evk%3A%2F%23%20cp%20%2Fetc%2Flibnfc-nci.conf%20%2Fusr%2Flocal%2Fetc%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CBR%20%2F%3E%0A%3CP%3ENow%2C%20you%20can%20run%20the%20nfcDemoApp%20on%20the%20i.MX6ULL%20EVK.%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3Eroot%40imx6ull14x14evk%3A%2F%23%20cd%20.libs%2F%0Aroot%40imx6ull14x14evk%3A%2F.libs%23%20.%2FnfcDemoApp%20poll%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22nfcDemoApp.png%22%20style%3D%22width%3A%20933px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22nfcDemoApp.png%22%20style%3D%22width%3A%20933px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F312581iC068E36E59F0B4DD%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22nfcDemoApp.png%22%20alt%3D%22nfcDemoApp.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CBR%20%2F%3E%0A%3CP%3EReferences%3A%3C%2FP%3E%0A%3CP%3E1.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com.cn%2Fdocs%2Fen%2Fuser-guide%2FIMX_YOCTO_PROJECT_USERS_GUIDE.pdf%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ei.MX%20Yocto%20Project%20User's%20guide%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E2.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com.cn%2Fdocs%2Fen%2Fapplication-note%2FAN13287.pdf%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EPN7160%20Linux%20Porting%20Guide%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E3.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DMCIMX6ULL-EVK_DESIGNFILES%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3E%3CSPAN%20class%3D%22meta-item%22%3EMCIMX6ULL-EVK_DESIGNFILES%3C%2FSPAN%3E%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E4.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdownloads%2Fen%2Fboard-support-packages%2FHW6635.zip%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EOM27160A1HN%20Hardware%20Design%20Files%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E5.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdownloads%2Fen%2Fboard-support-packages%2FHW6707.zip%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EOM29110%20NFC%E2%80%99s%20SBC%20Interface%20Board%20Design%20Files%3C%2FA%3E%3C%2FP%3E%0A%3CP%3E6.%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fi-MX-Processors-Knowledge-Base%2FPN7150-NFC-Controller-on-i-MX8M-mini-evk-running-Yocto%2Fta-p%2F1125177%22%20target%3D%22_self%22%3EPN7150%20NFC%20Controller%20on%20i.MX8M%20mini%20evk%20running%20Yocto%3C%2FA%3E%3C%2FP%3E%0A%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1994337%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3EContact%20Smart%20Card%20Reader%20ICs%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E
No ratings
Version history
Last update:
‎11-26-2024 07:15 PM
Updated by: