DISCLAIMER APPLICABLE TO THIS DOCUMENT CONTENTS:
This post contains a guide of how to use i.MXRT1050 demoboard with other NXP demoboards to demonstrate Secure access to industrial IOT, using NFC, embedded secure element and MCU (see picture below). A ready to use package including preparation of a secure element, and of a MIFARE DESFire EV2 card can be used as 3-step authentication example using symmetric AES keys; a session key will be generated inside SE050 which will be exported to i.MXRT1050 which will handle contactless communication thru CLRC663 plus frontend.
This document is structured as follows:
Following hardware is required to run the project:
The i.MXRT1050 EVKB development board provides the ideal platform for evaluation of and development with the i.MX RT1050 crossover processor, featuring NXP’s advanced implementation of the Arm® Cortex®-M7 core. The i.MX RT1050 EVK is a 4-layer through-hole USB-powered PCB. The board includes a high performance onboard debug probe, audio subsystem and accelerometer, with several options for adding off-the-shelf add-on boards for networking, sensors, display and other interfaces.
This core operates at speeds up to 600 MHz to provide high CPU performance and best real-time response.
Support for Amazon FreeRTOS™ available within the MCUXpresso SDK.The i.MX RT1050 EVK board is now supported by Arm® Mbed™ OS and Zephyr™ OS, both open source embedded operating systems for developing the Internet of Things.
| i.MX RT Series |
|
| 6-Axis |
|
| USB PD-PHY and CC-Logic |
|
| Load Switches |
|
The i.MXRT1050 EVKB is fully supported by the MCUXpresso suite of tools, which provides device drivers, middleware and examples to allow rapid development, plus configuration tools and an optional free IDE. MCUXpresso software is compatible with tools from popular tool vendors such as Arm and IAR, and the i.MXRT1050 EVKB may also be used with the popular debug probes available from SEGGER and P&E Micro.
As final touch to this demonstrator, one LCD display will be added in order to show "access control" check result when approaching a MIFARE DESFire EV2 card to the Reader antenna, without the use of a computer console.Connection between i.MXRT1050 EVKB board and LCD Display requires attachment of two flat cables, one for touch-screeen functionality and the other for controlling Display itself.
Click here to order Touchscreen LCD Display thru buy direct: P/N: RK043FN02H-CT 12NC:935358709598
It is easier to use the BLE-NFC-V2 board due to four Arduino compliant male connectors. Current version has only double row-male connectors which imposes that BLE-NFC-V2 board will be the last board stacked on top of other arduino boards. The following figure shows the pin mapping between the two boards.
|
Pin Function |
i.MXRT1050 (Arduino connector # - Pin #) |
CLRC663 plus |
NFC BLE V2 (Arduino connector # - Pin #) |
|
MOSI |
J24-5 |
MOSI |
J10-P14 |
|
MISO |
J24-4 |
MISO |
J10-P12 |
|
SPI CLK |
J24-6 |
SCK |
J10-P10 |
|
SPI CS |
J24-3 |
SSEL |
J10-P16 |
|
RESET |
J22-6 |
CLRCL_NRST |
J12-P6 |
|
IRQ |
J22-5 |
IRQ |
J12-P8 |
|
IFSEL0 |
J24-7 GND |
IF0 |
Via R11 |
|
IFSEL1 |
J25-4 VCC |
IF1 |
Via R9 |
|
GND |
J25-6 GND |
GND |
J11-P11 |
The OM-SE050ARD is the flexible and easy-to-use development kit for the EdgeLock™ SE050 Plug & Trust product family. It can be used in various ways for example via the Arduino interface compatible to any board featuring an Arduino compatible header, including many i.MX, LPC and Kinetis® boards, or via a direct I2C connection. This kit allows evaluation of the SE050 product family features and simplifies the development of secure IoT applications. More information can be found in the respective Application Note AN12395.
It is necessary to short circuit 4 empty resistor pads: R278, R279, R280 and R281 – they connect SPI from i.MX1050 until Arduino SPI pads, which will be used by NFC BLE V2 board.
It is necessary to cut at least one male pin to avoid conflict with OM-SE050ARD board (better would be to cut first 2 pins):
Since NFC BLE V2 has only male connectors, OMSE050ARD board is first connected to i.MX1050 EVKB, then NFC BLE V2 is plugged on top of this latest pcb.
Preparation of MFDFEV2 card
The touch screen display will offer three functionalities. By default, the first screen will be "Authenticate" functionality. When you choose the arrow to the right, you'll find TAB with word START, that you'll touch when you need to prepare a MIFARE DESFire EV2 card with suitable application and AES keys used for demonstrator. Just place a virgin card on top of Reader antenna, and press "START" button and check with Terminal on MCUxpresso to check sequence of actions to personalize one DESFire EV2 card. You may also use Teraterm to monitor the execution of DESFire card personalization, by inspecting the COM number used by i.MXRT1050 board.