PN5190/PN7642 - LPCD evaluation in NFC Cockpit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190/PN7642 - LPCD evaluation in NFC Cockpit

PN5190/PN7642 - LPCD evaluation in NFC Cockpit

LPCD (Low Power Card Detection) works on the principle that the I and Q values are extracted from the RF signal captured on the RX pins. These values are then compared with the I and Q data obtained using LPCD calibration. If the difference is greater than the chosen I and Q threshold, the load is detected and the IC wakes up. 

1// LPCD Way of working 

  • Run LPCD Calibration 
    • It is recommended to use an external power supply to supply the EVK board. If the USB supply is used, the value can fluctuate because of the transition effects. 
  • Run "Single LPCD" and check the performance 
  • Adjust the I and Q thresholds 
    • Low value -> Better detection range, more false wake-ups 
    • High value -> Worse detection range, fewer false wake-ups 

The number of samples, RSSI, and VDDPA parameters typically remain at their default values. 

Tomas_Parizek_0-1758116172644.png

2// Auto LPCD 

When the "Auto LPCD" is used, the LPCD algorithm always performs LPCD Calibration before entering the LPCD.

Tomas_Parizek_2-1758117682336.png

3//Semi-autonomous LPCD mode (PN5190 only)  

The user can evaluate the I and Q values behaviour under loaded/unloaded conditions. Based on that, the LPCD threshold can be properly selected. 

  • Use the same "Register" RSSI Target and Hysteresis as for "EEPROM"
  • Calibrate LPCD
  • Run "Endless I/Q read" 
  • Check how the I and Q values change
    • With no card/object in the antenna proximity 
    • with a NFC card/object in the antenna proximity

Tomas_Parizek_3-1758117823769.png

Labels (1)
No ratings
Version history
Last update:
‎09-19-2025 12:10 AM
Updated by: