How To Update PN7462 Firmware On Windows/Ubuntu PC/iMX8MN-EVK with Embeded Linux BSP Via USB port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Update PN7462 Firmware On Windows/Ubuntu PC/iMX8MN-EVK with Embeded Linux BSP Via USB port

How To Update PN7462 Firmware On Windows/Ubuntu PC/iMX8MN-EVK with Embeded Linux BSP Via USB port

--The document consists of the following:

Step 1. Connections And Firmware Version
Step 2. Updating FW On PC Windows 10
Step 3. Updating FW On VMplayer16.0 + Ubuntu 20.04
Step 4. Updating FW On i.MX8MN-EVK With Embedded L5.4.70_2.3.0 BSP
Step 5. Confirming whether update is successful using cockpit4.8

--About Cockpit

There are several different versions of cockpit, and each version can only recognize the same version of firmware.

--Reference Materials

1.https://community.nxp.com/t5/NFC/Mounting-the-PN7462AU-in-the-USB-downloader-mode-under-Linux/m-p/80...

2.https://community.nxp.com/t5/NFC/PN7462-updating-EEPROM-on-linux/m-p/739808/highlight/true#M3144

 

 

 

NXP CAS-TIC team

Weidong Sun

04-15-2021

 

Attachments
No ratings
Version history
Last update:
‎04-14-2021 08:29 PM
Updated by: