Dear S32DS and RTD team,
I installed S32K5 RTD 0.8.1 CD01 onto S32DS 3.6.6, but I'm not able to see the S32K5xx folder at "Create S32DS Project from Example" wizard.
Below is the other packages installation status. Would you please advise me if there were any other missing package to generate the example project in S32K5 RTD 0.8.1 CD01?
Best regards,
Yuji
Hi @YujiMizuishi
In release notes of this release:
===================================== Examples ===================================== Examples are not delivered in this release.
There's no example included in this package so you can't find it available
Hi @cuongnguyenphu,
I thought RTD 0.8.1 CD01 P01 had one example for Crypto_43_HSE_TS module. Can we generate this example on S32DS?
Best regards,
Yuji
I haven't checked this version RTD 0.8.1 CD01 P01, but if it released with an example then of course you can use it