2053398_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2053398_en-US

2053398_en-US

How to Set Up CS2100 and Configure PTA26 on S32K344 to Enable STGL5000?

Hello, all

I 'm working with the S32K344 WB and trying to enable the STGL5000.
According to the STGL5000 datasheet, the SYS_MCLK pin needs a clock signal before activation.

스크린샷 2025-02-28 113050.png

However, in the provided example Sound Mixer Release Pack, I couldn't find any setup for generating the clock signal on SYS_MCLK using CS2100CP.

스크린샷 2025-02-28 113333.png

I have the following questions:

  1. How can I properly configure CS2100CP to provide the necessary clock signal for SYS_MCLK?
  2. How should I set up PTA26 on the S32K344 to output the clock signal correctly?

Any guidance, example code, or register configuration detail


s would be greatly appreciated.

Thank you!

Re: How to Set Up CS2100 and Configure PTA26 on S32K344 to Enable STGL5000?

Hi

Are you referring to the Sound Mixer Release Pack.zip attached in S32K Sound Mixer?
S32K Sound Mixer User Guide.pdf mentions:
The S32K Sound Mixer demo includes K3 and K1 series, the test HW are listed below:
S32K3x4EVB-Q257
S32K148-T-BOX

Sorry, due to the hardware differences between S32K3x4EVB-Q257 and S32K344-WB you are using, you cannot run that project directly.
It is recommended that you download S32K344_Whiteboard_Example_RTM_1.0.0.zip in S32K344 Whiteboard Example Project.
It contains the Sai_47478A_440_100 project meet your need.
C:\NXP\S32K344_Whiteboard_Example_RTM_1.0.0\S32K344_Whiteboard_Example_RTM_1.0.0\SAI\Sai_47478A_440_100

Sai_47478A_440_100 Sgtl5000_Cs2100 S32K344_Whiteboard_Example_RTM_1.0.0.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 04:28 PM
更新者: