1932913_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1932913_en-US

1932913_en-US

SJA1124 (SPI to LIN)

Hello, nxp has a SJA1124 that provides an SPI to LIN chip. Please do you have any information about the chip and driver code, etc., and if so, can you provide it to me, thank you very much!

Re: SJA1124 (SPI to LIN)Hello Thomas, I am currently unable to establish normal communication with the sja1124 chip. I want to develop a Linux driver adapted to the sja1124 chip, but I can't read the data through the function interface provided by the Linux driver, I want to know if there is any specific pin state when the chip is working normally, can you help me?Re: SJA1124 (SPI to LIN)Hello Tomas, thank you for your reply, I got a part of the information according to your prompt, which helped me a lot!Re: SJA1124 (SPI to LIN)

Hi,

Thank you for your interest in the SJA1124 SPI-to-LIN bridge with four LIN commander channels.

I believe you can find useful the following items which are available as Secure Files (requiring an NDA) on the SJA1124 website:

https://www.nxp.com/products/interfaces/automotive-lin-solutions/quad-lin-commander-transceiver-with...

1. SJA1124 - Example software package including the example application and SJA1124 software driver.

1.png

2. AH1705 (AH504214 - SJA1124 / TJA1124 Application Hints (1.5))

2.png

PS: If your company has not signed the NDA with NXP yet, you can request it from:
https://www.nxp.com/support/support:SUPPORTHOME

Please make sure you are signed in to nxp.com. If you do not see these items, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. For more information about secure access rights, please refer to this website:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS

BRs, Tomas

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:37 PM
Updated by: