update target of freemaster

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

update target of freemaster

1,822 次查看
David_Qin___1
Contributor I

Hello,

When I use freemaster with MCAT, if I modify the "F0"(or ) then click the "Update Target" , I will see the following error, why? it is the official GUI.

The FreeMASTER version is v3.1.3.8

Oliver_Zhang_0-1640854080458.png

Thanks.

 

0 项奖励
回复
3 回复数

1,788 次查看
nxf45548
NXP Employee
NXP Employee

@David_Qin___1 , 

I mean by part number, the hardware that you are using. Are you using an LPC, Kinetis, iMxRT product? 

Regards

0 项奖励
回复

1,816 次查看
nxf45548
NXP Employee
NXP Employee

Thank you for contacting NXP Technical support. 
To provide you with better support, can you please let us know the part number that you are using? 

0 项奖励
回复

1,811 次查看
David_Qin___1
Contributor I

@nxf45548 

Hello,

Can you tell me what is the part number? thanks!

0 项奖励
回复