update target of freemaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

update target of freemaster

1,837 Views
David_Qin___1
Contributor I

Hello,

When I use freemaster with MCAT, if I modify the "F0"(or ) then click the "Update Target" , I will see the following error, why? it is the official GUI.

The FreeMASTER version is v3.1.3.8

Oliver_Zhang_0-1640854080458.png

Thanks.

 

0 Kudos
Reply
3 Replies

1,803 Views
nxf45548
NXP Employee
NXP Employee

@David_Qin___1 , 

I mean by part number, the hardware that you are using. Are you using an LPC, Kinetis, iMxRT product? 

Regards

0 Kudos
Reply

1,831 Views
nxf45548
NXP Employee
NXP Employee

Thank you for contacting NXP Technical support. 
To provide you with better support, can you please let us know the part number that you are using? 

0 Kudos
Reply

1,826 Views
David_Qin___1
Contributor I

@nxf45548 

Hello,

Can you tell me what is the part number? thanks!

0 Kudos
Reply