I tried to update AMMIC lib from 0.9 to AMMIC lib from 0.9 to MPC564xL_AMMCLIB_v1.1.23 for SPC5643L in code warrior 11. got the attached information,it seams theres is wrong pathes,i update the pathes setting as the same as the MTRCKTSPS5643L_SW which is for S32DS. i got errors too,
i check the MPC564XLMCLUG.PDF, it says i should enable SPE in the interrupt for SPC5643L,can anyone help me?
Hello,
Could you please elaborate the issue closely and post full screenshots of errors reported by compiler?
So you are migrating SPC5604 project? Which SPEC5604B or P ?
Best regards,
Peter
Hello,
Make sure you correctly set paths to your header files in S32DS.
If possible post full screenshots of the errors with paths.
check the MPC564XLMCLUG.PDF, it says i should enable SPE in the interrupt for SPC5643L,can anyone help me?
You have to modify your interrupt handler prolog.
As the MSR content will not reflect SPE bit, once you enter interrupt and will be restored on return from interrupt.
So if you want to use SPE functions in interrupt make sure SPE is enabled in MSR register in your interrupt.
Best regards,
Peter
i can not fix the errors,my SPC5643L firmware project is migrate from SPC5604 firmware project . there must be something that can not compatible for the new MPC564xL_AMMCLIB_v1.1.23 ?