example NXP S32K Position FOC control mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

example NXP S32K Position FOC control mode

2,058 次查看
michelet1
Contributor II

hello,

i would need to add position FOC control mode to a motor control example for s32k1.

I wanted to take hint from an existing example but i didn't find any NXP examples for motor control s32k that implemented position control. Do you know if there are any examples to start from?

Thanks in advance

 

3 回复数

2,040 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

All the examples available about S32K1 you can find in MCSPTE1AK144.

Hope it helps you.

Have a nice day!

0 项奖励
回复

2,021 次查看
michelet1
Contributor II

Hi,

thank you for your reply.

Right now i'm already using the project MCSPTE1AK144.

However, this project does not include position FOC control.

Are there other motor control projects of the s32k(k1,k3 ect...) which include position foc?

just to take a cue from a position control already created also to see which functions of the Automotive math and Motor Control library(MLIB,AMCLIB etc...) it uses to create position control.

Any point to understand how to implement a position control within the project MCSPTE1AK144 would be very useful and interesting for me.

Thanks again for your help.

0 项奖励
回复

2,007 次查看
_Leo_
NXP TechSupport
NXP TechSupport

The examples of the MCSPTE1AK344 are also available, but they also do not include the position FOC control.

Sorry for the inconvenience.

0 项奖励
回复