When we can get freeRTOS+TCP/UDP with PMSM FOC reference design base on KV5x ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When we can get freeRTOS+TCP/UDP with PMSM FOC reference design base on KV5x ?

1,924 Views
sungbryan
Contributor I

When we can get freeRTOS+TCP/UDP with PMSM FOC reference design base on KV5x ?

Labels (1)
0 Kudos
Reply
2 Replies

1,362 Views
pietrodicastri
Senior Contributor II

Hei

If You want to answer after so long time to this post, 

let me know where the RTOS and LWIP is available for the KV5x. I tried to download the TWR-KV58F220M

KSDK with all the options enabled, and there is no RTOS and LWIP example in.

Help??

Thank You

Pietro

0 Kudos
Reply

1,362 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bryan,

Yes, it is okay to get the freeRTOS+TCP/UDP with PMSM FOC reference design base on KV5x.

You can download the SDK2.0 based on KV5x from the website:

Welcome to Kinetis Expert | Kinetis Expert

after you download SDK, you can see the LWIP example code in the directory:

C:\DriverE\Freescale\KSDK1.2.0_KV5xF_1.0.0\examples\twrkv58f220m\demo_apps\lwip

each LWIP example includes two version:bare mental and FreeRTOS, you can use the example as platform and add the PMSM code, it is okay.

For the PMSM code based on FOC, you can download it from website:

3-Phase PMSM Motor Control Reference Design|NXP

Hope it can help you.

BR

Xiangjun Rong

0 Kudos
Reply