S912ZVC19F0VLFR 能用S912ZVCA19F0VLFR替代?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVC19F0VLFR 能用S912ZVCA19F0VLFR替代?

768 Views
Caleb1
Contributor I

S912ZVC19F0VLFR 能用S912ZVCA19F0VLFR替代?软件方面需要注意什么?

0 Kudos
Reply
1 Reply

744 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

They are absolutely the same physically – they have the same mask set. But the difference is related to set of defined peripheral (influences tests procedures) – you are not allowed to use undefined memories, peripherals or features.

So, in the case of the same mask set and in the case of these two devices it is enough for you to look at the table Table 1-1. MC9S12ZVC-Family devices.

S912ZVC = Standard (10Bit ADC, no DAC, no Comparator)
S912ZVCA= Enhanced analog(12Bit ADC, with DAC & Comparator

 

ZVCA               vs              ZVC
12 bit ADC                     10bit ADC
8bit DAC                            NA
ACMP 5V                           NA

 

In this case, however, you want to use device with extended features so just check ADC setup.


Best regards,

Ladislav

0 Kudos
Reply