Hello,
Is it possible to use MCRSP_PMSM_V1.2.0 with LPC15xx?
Best Regards,
Peter
Solved! Go to Solution.
Hello Peter,
You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:
This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal
Note: This firmware contains FOC control of PMSM motor in QEI sensored mode
Best Regards,
Sabina
Hello,
This release has been on and supports the following development platforms:
Unfortunately, this does not include the LPC.
Best Regards,
Sabina
Hi Sabina,
Thank you for the replay.
If there is some example project with LPC15xx and FOC (without MCRSP_PMSM)?
Best Regards,
Peter
Hello Peter,
You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:
This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal
Note: This firmware contains FOC control of PMSM motor in QEI sensored mode
Best Regards,
Sabina
Hi Sabina,
Thank you very much!
Best Regards,
Peter