MCRSP_PMSM_V1.2.0 with LPC15xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCRSP_PMSM_V1.2.0 with LPC15xx

Jump to solution
2,399 Views
peterkostadinov
Contributor III

Hello,

Is it possible to use MCRSP_PMSM_V1.2.0 with LPC15xx?

Best Regards,

Peter

Labels (1)
Tags (1)
0 Kudos
1 Solution
2,297 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Peter,

You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:

This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal

Note: This firmware contains FOC control of PMSM motor in QEI sensored mode

Best Regards,

Sabina

View solution in original post

0 Kudos
4 Replies
2,297 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

This release has been on and supports the following development platforms:

pastedImage_1.png

Unfortunately, this does not include the LPC.

Best Regards,

Sabina

0 Kudos
2,297 Views
peterkostadinov
Contributor III

Hi Sabina,

Thank you for the replay.

If there is some example project with LPC15xx and FOC (without MCRSP_PMSM)?

Best Regards,

Peter

0 Kudos
2,298 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Peter,

You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:

This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal

Note: This firmware contains FOC control of PMSM motor in QEI sensored mode

Best Regards,

Sabina

0 Kudos
2,297 Views
peterkostadinov
Contributor III

Hi Sabina,

Thank you very much!

Best Regards,

Peter

0 Kudos