MCAT for two motors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCAT for two motors

1,593 次查看
peterkostadinov
Contributor III

Hi All,

I'm using an example project from "MCRSP_PMSM_V1.2.0" and also FreeMaster+MCAT "pmsm_ref_sol.pmp". For my application I need to handle parameters for two PMSM motors in one FreeMaster+MCAT project. According to the datasheets it is possible, but in "pmsm_ref_sol.pmp", the motor selector bar is missing. 

Best Regards,

Peter

0 项奖励
回复
2 回复数

1,456 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Peter,

 

You may want to take a look to the following application note, it could give you an idea of how to implement it.

Dual Motor Control for PMSM with the Kinetis K70

 

Please find code attached.

 

Best regards,

Felipe

0 项奖励
回复

1,456 次查看
peterkostadinov
Contributor III

Hi Filipe,

Thank you very much for the information provided. Your answer is not exactly related to my question about 2 motors in one FreeMaster + MCAT project (see the picture below), but it still gives me very valuable guidance in my work.

Untitled.png

Best Regards,

Peter

0 项奖励
回复