MC33887 Output avalanche protection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33887 Output avalanche protection

1,723 Views
WolfgangCS
Contributor I

Hello,

In the datasheet of the "MC33887 5.0 A H-bridge with load current feedback" there is a section on "Output avalanche protection" on page 21 of the pdf file (see attachment), which suggests using "a zener clamp and/or an appropriately valued input capacitor with sufficiently low ESR" on the V+ input.

If the zener diode is used, how should it be connected? In parallel with the input capacitor? With the anode connected to ground and the cathode to V+? 

Thank you very much

Tags (1)
0 Kudos
Reply
2 Replies

1,718 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:If the zener diode is used, how should it be connected? In parallel with the input capacitor? With the anode connected to ground and the cathode to +V?

[gw]Correct!

1,711 Views
WolfgangCS
Contributor I

Thank you for your reply.
If a V+ voltage of 24V is used, what type of Zener diode could be used?

0 Kudos
Reply