Similar to this link, https://us.flukecal.com/products/ele...wer-calibrator
My current design might be class AB type.
I am not worried to much about PWM generation ruther I am thinking how can I move class AB to Class D amplification.
A lot of the design effort relates to maintaining linearity and avoiding crossover distortion.
2 amplifiers( current, voltage) output will feed to CT and PT!
REQUIRMENTS :
1. The amp input should be plus and minus 7volt AC, 45-65Hz( 1 Hz has been converted to 1024)
2. Amp operating voltage should be more or less 24v.
3. 2 channel signal (not sure PWM) should be use , one for current, one for voltage.
4. Can run current transformer(input 16.5 V/1.5 A) and potential Transformer (input15v/2A). PT output may be 15VAC.
5. If possible both voltage and current amplification is required in one IC.
6. Both positive and negative half signal should be amplify.
HI
Unfortunately we don't have suitable devices for recommend,if any questions please let us know!
Could you have anything for short circuit protection in/out of transformer as I have mentioned ?
From your experience kindly suggest a way to get a solution then.