In the "TWR-KV58F220M_Quick Start Package" there is a example in the "Precompiled Examples" called "pmsm_demos_twr-kv58f.bin" where is there the example KDS project for this binary?

cancel
Showing results for 
Search instead for 
Did you mean: 

In the "TWR-KV58F220M_Quick Start Package" there is a example in the "Precompiled Examples" called "pmsm_demos_twr-kv58f.bin" where is there the example KDS project for this binary?

1,231 Views
daledalke
Contributor I

The "pmsm_demos_twr-kv58f.bin" is a nice demo but would like to see the KDS project for this example. Did find the "Example source code for Kinetis 3 Phase BLDC Motor Control using TWR-MC-LV3PH", is this the project used?

Labels (1)
0 Kudos
3 Replies

790 Views
daledalke
Contributor I

I did finally fine this file "MCRSP_PMSM_V1.1.2" at this link "https://www.nxp.com/webapp/Download?colCode=MCRSP-PMSM&location=null&fsrch=1&sr=1&pageNum=1&Parent_n... " that contained the "pmsm_demo" for the "twr-kv58f". Was able to import the project, build and debug.

0 Kudos

790 Views
chris_brown
NXP Employee
NXP Employee

Hi Dale,

We didn't really have a KDS project when this package was created.  My suggestion for the official PMSM source is to view the Getting Started videos for motor control projects.  Please navigate to the TWR-KV58F220M Getting Started page​ and click on the Getting Started with the TWR-MC-LV3PH and TWR-KV58F220M​ link.

Please let me know if you have any trouble with these pages or comments. 

Thanks,

Chris

0 Kudos

790 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think you can download the PMSM FOC control with sensorless from the website:

http://tinyurl.com/hxgtc63

But I am not sure if it is the same prject the doc mentioned.

Hope it can help you

BR

Xiangjun rong

0 Kudos