56F8013 - 48V Sensorless Acim

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56F8013 - 48V Sensorless Acim

2,956件の閲覧回数
carlo_54
Contributor I

Hi, I'm trying to make a 48V ACIM sensorless driver. I would like to use the dsp 56F8013. The DRM075 application shows a project in Code Warrior 8.3 called "Third.mcp", but I can't find it available on the NXP site. Can someone help me ? Thank you

0 件の賞賛
8 返答(返信)

1,098件の閲覧回数
stevediaz
Contributor I

Hello

To obtain the necessary project files and resources for your specific application, I recommend reaching out directly to NXP Semiconductor's technical support or visiting their official website. They should be able to provide you with the latest documentation, software, and project files related to the DRM075 application and the 56F8013 microcontroller.

Check below steps:

  1. Navigate to the "Support" or "Downloads" section.

  2. Use the search or browse features to find resources related to the DRM075 application and the 56F8013 microcontroller.

  3. If you can't find the specific project file you're looking for, contact NXP's technical support or customer service for assistance. They can guide you to the right resources or provide additional support.

https://www.nxp.com/design/designs/kv-series-3-phase-ac-induction-motor-control:THREE-PHASE-AC-INDUC...Power BI Certification

Thank you.

0 件の賞賛

2,866件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked the AE team, unfortunately the firmware based on DRM075 is unavailable, nobody can find it out in archive, I suggest you refer to the ACIM example based on KV family. The code is developed in C, so it adapts to both DSC and KV.

 

https://www.nxp.com/design/designs/kv-series-3-phase-ac-induction-motor-control:THREE-PHASE-AC-INDUC...

BR

XiangJun Rong

0 件の賞賛

2,951件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the code, hope it can help you

BR

XiangJun Rong

0 件の賞賛

2,938件の閲覧回数
carlo_54
Contributor I

Hi

Thanks, but I looked at the code and  is sensored, it uses the incremental encoder. The program I am looking for has the name "Thirdp.mcp", it is acim sensorless. I tried to use the code "CloseV07.mcp" but it seems to have problems ....

0 件の賞賛

2,932件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to check this one.

BR

XiangJun Rong

0 件の賞賛

2,896件の閲覧回数
carlo_54
Contributor I

Hi
Isn't there really a  56F8013 sample program for  ACIM sensorless driver in the NXP archives?
I can't find it
Thank you

BR

0 件の賞賛

2,924件の閲覧回数
carlo_54
Contributor I

Hi.

Thank you very much, but there is an error. The attachment is the hardware circuit of the motor control circuit, not the Foc acim sensorless software. If the software for the 56F8013 is  to buy only, no problem, I can buy it.
BR

Giancarlo

0 件の賞賛

2,943件の閲覧回数
carlo_54
Contributor I

Thanks so much !

0 件の賞賛