User manual sasy: "The s-record file that needs to be manually programmed into the MCU is MPC564xL.rbf" and then:
"It is located in the MCD Toolbox installation directory under: ...\tools\BootLoader\RBF_Files."
As I see there is no such file in this directory. There is only .rba (RAM) file in the RBA_Files folder. Is it mistake in the User Guide ? How should we prepare/configure board to use it with PIL simulation ?
In case of using .rba file: does it matter if we use MPC564xL.rba or PXS20xx.rba to work with TWR-PXS2010 board ?
Thanks for help
Maciek
解決済! 解決策の投稿を見る。
- For the MPC564xL there is no RBF file. The for the MPC564xL there is only a RBA file used.
- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.
- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode. That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0. Please see the MPC564xL Reference Manual chapter 9 for more details.
- For the MPC564xL there is no RBF file. The for the MPC564xL there is only a RBA file used.
- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.
- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode. That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0. Please see the MPC564xL Reference Manual chapter 9 for more details.