where to look for MPC564xL.rbf file ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where to look for MPC564xL.rbf file ?

ソリューションへジャンプ
3,212件の閲覧回数
Maciek
Contributor V

User manual sasy: "The s-record file that needs to be manually programmed into the MCU is MPC564xL.rbf" and then: 

"It is located in the MCD Toolbox installation directory under: ...\tools\BootLoader\RBF_Files."

As I see there is no such file in this directory. There is only .rba (RAM) file in the RBA_Files folder. Is it mistake in the User Guide ? How should we prepare/configure board to use it with PIL simulation ?

In case of using .rba file: does it matter if we use MPC564xL.rba or PXS20xx.rba to work with TWR-PXS2010 board ?

Thanks for help

Maciek 

0 件の賞賛
返信
1 解決策
2,821件の閲覧回数
john_floros
NXP Employee
NXP Employee

- For the MPC564xL there is no RBF file.  The for the MPC564xL there is only a RBA file used. 

- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.

- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode.  That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0.  Please see the MPC564xL Reference Manual chapter 9 for more details.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,822件の閲覧回数
john_floros
NXP Employee
NXP Employee

- For the MPC564xL there is no RBF file.  The for the MPC564xL there is only a RBA file used. 

- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.

- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode.  That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0.  Please see the MPC564xL Reference Manual chapter 9 for more details.

0 件の賞賛
返信