where to look for MPC564xL.rbf file ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where to look for MPC564xL.rbf file ?

Jump to solution
3,227 Views
Maciek
Contributor V

User manual sasy: "The s-record file that needs to be manually programmed into the MCU is MPC564xL.rbf" and then: 

"It is located in the MCD Toolbox installation directory under: ...\tools\BootLoader\RBF_Files."

As I see there is no such file in this directory. There is only .rba (RAM) file in the RBA_Files folder. Is it mistake in the User Guide ? How should we prepare/configure board to use it with PIL simulation ?

In case of using .rba file: does it matter if we use MPC564xL.rba or PXS20xx.rba to work with TWR-PXS2010 board ?

Thanks for help

Maciek 

0 Kudos
Reply
1 Solution
2,836 Views
john_floros
NXP Employee
NXP Employee

- For the MPC564xL there is no RBF file.  The for the MPC564xL there is only a RBA file used. 

- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.

- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode.  That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0.  Please see the MPC564xL Reference Manual chapter 9 for more details.

View solution in original post

0 Kudos
Reply
1 Reply
2,837 Views
john_floros
NXP Employee
NXP Employee

- For the MPC564xL there is no RBF file.  The for the MPC564xL there is only a RBA file used. 

- MPC564xL.rba and PXS20xx.rba are identical and therefore either can be used.

- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode.  That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0.  Please see the MPC564xL Reference Manual chapter 9 for more details.

0 Kudos
Reply