"PART 15: Processor-in-the-Loop (PIL) Validation" on S12ZVML12EVBLIN issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"PART 15: Processor-in-the-Loop (PIL) Validation" on S12ZVML12EVBLIN issue

跳至解决方案
1,625 次查看
ngoctuhoang
Contributor II

Dear MBD team,

With youtube tutorial "PART 15: Processor-in-the-Loop (PIL) Validation" https://www.youtube.com/watch?v=JSabErrV4M8&list=PLd9y9YP-KUTB4OZ31XKLjXMLu9rV0Eh-d&index=16&t=0s

I adapt the example model (Lecture7_MPC5744P_v3.2.0.zip) to use with S12Z. But somehow it does not work.

Top Level Model:

Top level.PNG

PIL_block:

PIL_block With Config.PNG

Configuration Parameters setting is the same for both Top level and PIL Model:

PIL_block_CodeGen.PNG

PIL_block_HW_Impleme.PNG

When I do the step "Tools/..../To PIL Mode on S12Z", I get error:

To_PIL_error.bmp

toPIL_error.PNG

Could you help me please?

Toolchains:

Matlab/Simulink 2017a

Motor Control Development Toolbox for MagniV S12Z    Version 1.3         (R2013a-R2015b)

Code Warrior Version: 11.0.1

Many thanks in advance!

BR

Tony

0 项奖励
回复
1 解答
1,519 次查看
ngoctuhoang
Contributor II

Maybe is helpful for someone newbie like me in NXP-S12Z MBD Toolbox.

I try with Matlab 2015a, and It works.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,520 次查看
ngoctuhoang
Contributor II

Maybe is helpful for someone newbie like me in NXP-S12Z MBD Toolbox.

I try with Matlab 2015a, and It works.

0 项奖励
回复