problem with PIL simulation on NXPs32k144 evb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with PIL simulation on NXPs32k144 evb

1,478 Views
pierpaolo_dini
Contributor III

I encountering issues with concretize PIL procedure.

I face the following error in simulink

 

Cannot perform PIL simulation for "Esempio_0". Configuration parameters for this model do not support these connectivity configurations: IBIS_AMI, Arduino Board, Texas Instruments Code Composer Studio (IDE), Texas Instruments Code Composer Studio (TCP/IP), Texas Instruments Code Composer Studio (Serial), s32k_pil PIL, s32k_as_pil PIL Update configuration parameters or create a supported connectivity configuration. For more information, see Help Center.

 

i am sure that all the setup oprions are right (solver, settings i configure the HW implementation, th target block is right...), but i dont know why i face this error.

 

Its strange that if i build the code through the embedded coder app i face no problems in flashing the evb.

With harnest and SIL/PIL test apps instead i have such issue.

 

Can some one help me?

 

Thanks in advance

0 Kudos
Reply
2 Replies

1,443 Views
pierpaolo_dini
Contributor III

No one from technical support of NXP is able to provide solution or at least suggestion for workaround??!!

0 Kudos
Reply

1,413 Views
pierpaolo_dini
Contributor III

@paulvlase 

i remember you help me with another issue, so i invoke you.

Can you suggest something to do?

Thanks in advance.

0 Kudos
Reply