iMXRT: Noise on ADC_ETC Channels with SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT: Noise on ADC_ETC Channels with SDK

489件の閲覧回数
Sam_ECU
Contributor V

Hello,

I'm working with the imxrt1062 and trying to measure 7x pins on ADC1 and 6x pins on ADC2 using ADC_ETC.  The application is built from the MBDT/SDK Example for ADC_ETC.

It can be replicated on the EVK.

When previously tested, ADC_Polling, rather then ADC_ETC delivered the expected results.

I've tried to follow the info here but haven't managed to resolve my issue:
https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Trigger-ADC-with-PWM-on-IMX1064/td-p/1273086
https://www.nxp.com/docs/en/application-note/AN12214.pdf
https://community.nxp.com/t5/i-MX-Processors/ADC2-and-ADC-ETC-not-working-rt1024-evk/m-p/1336318
https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-ETC-sync-mode-questions-on-rt1050/m-p/844735

My issue is that several pins measure only noise, ADC2.IN.1 and ADC2.IN.2.

Sam_ECU_0-1731966506304.png

I can measure at the pins using a multimeter and they're a stable 3.3V. I can measure the "incorrect pins" with a neighbouring ADC (eg. Fuel_Level) and the values are correct. I can flash the code to the EVKB_1062 and see the same issue on the same channels so I'm sure that the issue isn't in the hardware.

My setup with the best results are:

ADC1:

Sam_ECU_1-1731966555169.png


ADC2:
Sam_ECU_2-1731966581605.png

ADC_ETC:

Sam_ECU_3-1731966623683.png

Sam_ECU_4-1731966633442.png

I see no improvement or no measurements at all if I:
- ADC2: Set Trigger source to CH1_XBAR_TRG0 (Trigger Group 4)
- Remove "Bypass TSC"
- Change my PIT_Timer (1ms, 10ms, 100ms)
- Remove Back2Back and set delays and intervals
- Set ADC1_Channels as all Group 0 and ADC2_Channels as Group 1
- Change priorities
- Set up sync mode with ADC1 and Trigger Group 0 and ADC2 as Trigger Group 4

Here's the setup in Simulink to measure:

Sam_ECU_5-1731966818242.png

 

Sam_ECU_6-1731966852087.png


What am I missing? How can the issue be fixed to measure correctly all ADC1 and ADC2 channels.

Attached my Config.mex and Config Folder.  I can supply my whole program.

 

0 件の賞賛
返信
0 返答(返信)