can I use the FOC code developed by NXP for the Linux motor to control another type of motor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can I use the FOC code developed by NXP for the Linux motor to control another type of motor

ソリューションへジャンプ
2,260件の閲覧回数
abderrahimjamao
Contributor III

Good morning all,
I have a question, please. I am working on brushless motor control and want to know if I can use the FOC code developed by NXP for the Linux motor to control another type of motor. do I have to modify the code to adapt it with my motor or is it a general code?

タグ(1)
1 解決策
2,108件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

abderrahimjamaoui@gmail.com‌,

In general, if you only change the motor (i.e. Linix motor with another type of PMSM surface mount motor), you do not have to change the algorithm but you need to update the parameters of the motor and/or sensors.

Also, you need to retune the PI controllers for the new motor.

These are considered to be parameters for the FOC hence we can say that C-code does not change but the Data needs to be updated to have the motor running correctly.

Best regards,
Daniel

元の投稿で解決策を見る

4 返答(返信)
2,109件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

abderrahimjamaoui@gmail.com‌,

In general, if you only change the motor (i.e. Linix motor with another type of PMSM surface mount motor), you do not have to change the algorithm but you need to update the parameters of the motor and/or sensors.

Also, you need to retune the PI controllers for the new motor.

These are considered to be parameters for the FOC hence we can say that C-code does not change but the Data needs to be updated to have the motor running correctly.

Best regards,
Daniel

2,108件の閲覧回数
abderrahimjamao
Contributor III

ok, thank you so much. I don't understand how to retune the PI controllers for my motor.

0 件の賞賛
返信
2,108件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello abderrahimjamaoui@gmail.com,

I am not sure if you are referring to our models or other NXP code -- on this community we mainly handle topics regarding MATLAB/Simulink and our toolboxes. If you have specific questions regarding the examples we ship for FOC, adriantudor‌ can help with some answers.

Kind regards,

Razvan.

0 件の賞賛
返信
2,108件の閲覧回数
abderrahimjamao
Contributor III

Thanks, I'm sorry to ask the question in this community. 

0 件の賞賛
返信