Which MATLAB products were used for support MBDToolbox_S32K1xx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which MATLAB products were used for support MBDToolbox_S32K1xx?

2,880件の閲覧回数
weibing_liao
Contributor I

MATLAB has so many  products, like:

  • MATLAB
  • Simulink
  • MATLAB Coder
  • MATLAB Compiler
  • MATLAB Compiler SDK
  • MATLAB Report Generator
  • Simulink Check
  • Simulink Code Inspector
  • Simulink Coder
  • Simulink Compiler
  • Simulink Control Design
  • Simulink Coverage
  • Simulink Design Optimization
  • Simulink Design Verifier
  • Simulink Desktop Real-Time
  • Simulink PLC Coder
  • Simulink Real-Time
  • Simulink Report Generator
  • Simulink Requirements
  • Simulink Test
  • Stateflow
  • Statistics and Machine Learning Toolbox
  • Vehicle Dynamics Blockset
  • Vehicle Network Toolbox
  • Vision HDL Toolbox
  • ......

Which MATLAB products were used for support MBDToolbox_S32K1xx?

0 件の賞賛
返信
3 返答(返信)

2,605件の閲覧回数
Ahmed_BN
Contributor I

Hello @mariuslucianand ,

Sorry to ask again part of the question I have asked here, and to add a need for the dual motor kit.

I have a general question about the MathWorks code generator. We want to acquire small kits for BLDC control to develop RCP systems under the MathWorks environment : 
- MCSPTE1AK144 with S32K144
and
- MTRCKTDBN5643L with MPC5643L

And we ask if we just need :

( Matlab + Simulink + Stateflow ) + Embedded Coder ?

or do we need "Matlab Coder" and "Simulink Coder" in addition to Embedded Coder ? in other words :

( Matlab + Simulink + Stateflow ) + Embedded Coder + Matlab Coder + Simulink Coder ?

- Concerning the dual motor kit MTRCKTDBN5643L, I don't find explicitly a compatibility with the MBDT toolbox of NPX ? or maybe you have already provided links that explain this compatibility ?

Sincerely

 

0 件の賞賛
返信

2,836件の閲覧回数
weibing_liao
Contributor I

The following additional Toolboxes MATLAB Coder, Simulink Coder, and Embedded Coder ,Should we just have one or all of them?

0 件の賞賛
返信

2,872件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @weibing_liao,

Model-Based Design Toolbox for S323K1xx requires to have both MATLAB and Simulink and the following additional Toolboxes MATLAB Coder, Simulink Coder, and Embedded Coder. Without any of these, the code generation process will not work.

My suggestion is also to get the Stateflow toolbox because many of our models use some states transitions, and also might help you in your application.

Hope this helps,
Marius

0 件の賞賛
返信