Watchdog Error on S32CT (MBDT 1.4.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog Error on S32CT (MBDT 1.4.0)

1,033 Views
SuperBeginner
Contributor III

Dear NXP,

I want to configure Watchdog via Simulink.

I refer to this article:

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-implement-watchdog-for-S32K344-i...

Following his suggestion, I used S32DS to open WDG's Example Project to complete the configuration on S32CT.

WDG Example Project location is: TOOLBOX_ROOT\S32K3_RTD\SW32K3_RTD_4.4_R21-11_3.0.0\eclipse\plugins\Wdg_TS_T40D34M30I0R0\examples\S32DS\S32K3XX\Swt_Ip_Example_S32K344

Although I don't get any error on the S32CT configuration, I get an error on the Build Code.

WDG_ErrorMessage.PNG

The error message indicates that I am missing the file "AeWdog_Ip_Cfg_Defines.h"

But I can found "AeWdog_Ip_Cfg_Defines.h" in the example project, the path is
TOOLBOX_ROOT\S32K3_RTD\SW32K3_RTD_4.4_R21-11_3.0.0\eclipse\plugins\Wdg_TS_T40D34M30I0R0\generate\include

Can you help me troubleshoot this error?

 

I attach here my setup steps and environment.My setup up step is: 

1. Add Wdg tab: 

1.PNG

2.PNG

2. GPT Configuration:

3_GPT.PNG

4_GPT.PNG

5_GPT.PNG

6_GPT.PNG

3. MCU Configuration

7_MCU.PNG

8_MCU.PNG

9_Platform.PNG

10_Platform.PNG

4. WDG Configuration

11_WDG.PNG

12_WDG.PNG

13_WDG.PNG

14_WDG.PNG

15_WDG.PNG

5. Update Code:

16.PNG

My environment is S32K312EVB-Q172, MBDT 1.4.0, Matlab R2021a.

 

Thanks in advance

0 Kudos
Reply
2 Replies

1,002 Views
SuperBeginner
Contributor III

In addition to the above error, I found that I also got the following error:

WDG_ErrorMessage_2.PNG

But the difference is that I checked the Example Project and didn't find "WdgIf_Types.h".

Could you help me to solve this problem, please?

Thanks in advance

0 Kudos
Reply

979 Views
SuperBeginner
Contributor III

Dear NXP,

Could you please provide any assistance?

0 Kudos
Reply