[Warning] Wrong Configuration for PBRIDGE Clock in the MBD toolbox 3.0.0 - Devkit MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Warning] Wrong Configuration for PBRIDGE Clock in the MBD toolbox 3.0.0 - Devkit MPC5744P

ソリューションへジャンプ
2,144件の閲覧回数
rafael_barbosa
Contributor IV

Hello,

I am using the Devkit MPC5744P and I could check that the Model Based Design Toolbox 3.0.0 for Simulink has a wrong configuration for PBRIDGE clock.

By default, any model using the MBD toolbox presents the PBRIGDE clock frequency running on 100 MHz. I attached a model that verifies the clock configuration and a Freemaster file in order to make easier the visualization.

However the MPC5744P Reference Manual states that the maximum frequency configuration for PBRIGDE clock is 50 MHz, as can be checked below.

pastedImage_1.png

Kind Regards, Rafael Barbosa

mariuslucianandrei

1 解決策
2,063件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com,

I have attached here the new PEBRIDGE config.

The path for the file to be replaced is the following:

{TOOLBOX_DIR}\mbdtbx_mpc574x\src\c_library

Kind regards,

Razvan.

元の投稿で解決策を見る

2 返答(返信)
2,064件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com,

I have attached here the new PEBRIDGE config.

The path for the file to be replaced is the following:

{TOOLBOX_DIR}\mbdtbx_mpc574x\src\c_library

Kind regards,

Razvan.

2,063件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com‌,

I will investigate this issue and provide a fix for the correct value of PEBRIDGE clock.

Thank you for pointing this out!

Kind regards,

Razvan.