Use of Recorder with MCSXTE2BK142

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use of Recorder with MCSXTE2BK142

1,270 Views
E_S
Contributor II

Hello,

I want to look at some variables in a very high frequency (see Fig. 46 in https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Module-6-Current-Sensing-Part-2-2/m-p/7...). I have an MCSXTE2BK142.

From my understanding a scope is too slow for this job. Due to this I have to use the recoder. When I flash the FreeMaster Recorder example of the MBDT in Simulink to the Board (Project fm_s32k1xx), which demonstrates the FreeMaster Recorder Functionality, I get no values. This is the example where I changed the Targed Block and the FreeMaster Config for MCSXTE2BK142 (see attachment):

E_S_1-1648655143425.png

 

After some seconds in the FreeMaster scrren, there is the error "Stopped, waiting for acknowledge":

E_S_0-1648655029973.png

How can I use the recorder function? Is there a mistake in my configuration?

 

Furthermore I do not understand the placing of the "FreeMaster Recoder Call" Block in Simulink. Where do I have to place the block so that it works?

 

Thanks for your help!

0 Kudos
Reply
2 Replies

531 Views
Xiaowei_Chu
Contributor I

I have the very same problem, hope some NXP expert solve this.

0 Kudos
Reply

1,220 Views
iulian_stan
NXP Employee
NXP Employee

Hi @E_S,

I moved your question to MBDT community, because I cannot validate your MatLAB project and would like  someone from this community to take a look.

0 Kudos
Reply