Unable to run model on S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to run model on S32K312

706件の閲覧回数
AsierMaser
Contributor II

Hi everyone,

I am facing a problem when creating a project in Simulink. When I compile and deploy the model into the uC the program doesn't run. I have always used standard drivers instead of MCAL that are required for MBDT, so maybe some config is wrong. However, compared to the default config provided by the toolbox, it seems OK to me.

There are some drivers i didn't use, like EcuM or Os, which are not mandatory in theory, but when creating a project without them the build process shows different errors refering to these drivers, so I finally included them. Then I tried to configure both EcuM and Os the same way they are on the default config, but the program won't run. 

I am attaching the program I am using to check if the program runs or not; it is a simple CAN communication and led blinking.

Thanks,

BR

0 件の賞賛
返信
0 返答(返信)