Sleep Mode Implementation for S32K344.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sleep Mode Implementation for S32K344.

1,584 Views
GogateS
Contributor I

Hello,

I would like to know the procedure for implementing sleep mode on the S32K344 MCU using Simulink.

I can see that the necessary drivers are available in the S32 Configuration Tool, but I am not sure which MATLAB/Simulink toolbox or approach to use.

Could you please provide the step-by-step procedure for implementing sleep mode using Simulink for this MCU?

Thank You.

0 Kudos
Reply
1 Reply

1,192 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

I've created an article that shows how to put S32K344 into standby mode using Model Based Design Toolbox for S32K3 v1.8.0.  Please check How to: Standby mode on S32K3 using NXP MBDT for more information. Moreover, I've attached an example model that you can try. You might have to modify the pin used to wakeup the board and the pin used by the LED.

if you need other ways to wake up the board, you can also check the following article: S32K3 Low Power Management AN and demos .

 

Best regards,

Sorin Bancila