Simulink no configuration block for MPC57xx!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Simulink no configuration block for MPC57xx!

跳至解决方案
2,925 次查看
60010001
Contributor II

Screenshot (274).png

it occurs when i drag block model to workspace ,How to fix it?

I follow Quick Start Guide but didn't do 1.2.3 Setting up the Target Compiler because i don't know where it is.

1 解答
2,806 次查看
constantinrazva
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th,

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

在原帖中查看解决方案

3 回复数
2,807 次查看
constantinrazva
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th,

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

2,806 次查看
60010001
Contributor II

Thank you 

0 项奖励
回复
2,806 次查看
constantinrazva
NXP Employee
NXP Employee

Glad I could help you!

KR,

Razvan.