S32k144 not detecting analog input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k144 not detecting analog input

ソリューションへジャンプ
3,798件の閲覧回数
ba2nguye
Contributor I

Hello,

I am currently trying to make the S32K144 board to recognize an external analog signal in addition to multiple analog signals. (multiple sensors application)

I am running a 5-0V signal from a power supply to the NXP analog pins + potentiometer reading to see if my model can recognize multiple analog signals. However, I only obtain 2 readings of the NXP potentiometer and everything else is 0.

The algorithm should work as two independent readings of the potentiometer (analog) are working fine (with 2 separate memory slots in ADC).

I have attached the model below, including a FreeMaster file.

Thank you

0 件の賞賛
返信
1 解決策
3,602件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello ba2nguye@uwaterloo.ca‌,

My advice would be to check out the ftm_pdb_adc_chaining_s32k14x example - it comes with our toolbox, you can find it in S32_Examples/common/adc folder. There you have an example of how to synchronize ADC0 and ADC1 measurements with PWM commands issued by FTM via PDB. These 2 synchronized measurements are used to get the potentiometer value and the VDD LV value. You can read more about such techniques in Module 6: Current Sensing (Part 1/2)  article (quick references - figures 9, 10 and 11).

I have also attached an adc example in which the measurements are triggered by the PDB, like this:

- PDB is software triggered

- PDB triggers subsystem in which ADC measurements are made (on pins A0 and A1).

Hope this helps!

Razvan.

元の投稿で解決策を見る

5 返答(返信)
3,603件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello ba2nguye@uwaterloo.ca‌,

My advice would be to check out the ftm_pdb_adc_chaining_s32k14x example - it comes with our toolbox, you can find it in S32_Examples/common/adc folder. There you have an example of how to synchronize ADC0 and ADC1 measurements with PWM commands issued by FTM via PDB. These 2 synchronized measurements are used to get the potentiometer value and the VDD LV value. You can read more about such techniques in Module 6: Current Sensing (Part 1/2)  article (quick references - figures 9, 10 and 11).

I have also attached an adc example in which the measurements are triggered by the PDB, like this:

- PDB is software triggered

- PDB triggers subsystem in which ADC measurements are made (on pins A0 and A1).

Hope this helps!

Razvan.

3,592件の閲覧回数
rathi_tg
Contributor III

Hello Sir,

 

I have Performed an ADC test on pin number PTB6 and PTB7 on NXP S32K144 Evaluation Board.

 After the test the PinPTB7 works fine and the voltage varies from  0 to 5 volt as required. But, when the same test was performed on  pin PTB6 the values of the Pin do not vary.

Please let me know the reason if you face the same and solution to avaoid the problem 

Regards 

Gopal Rathi. 

 

0 件の賞賛
返信
3,589件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @rathi_tg ,

On the S32K144EVB, the PTB6 and PTB7 are used as XTAL PINS, connected to an *Mhz oscillator.

mariuslucianand_0-1603966224474.png

The pins on the J3 connectors are not connected to the processor, you can see those resister R81 and R90.

mariuslucianand_1-1603966269780.png

Hope this helps,

Marius

 

0 件の賞賛
返信
3,577件の閲覧回数
rathi_tg
Contributor III

Hello Marius 

 

I have mistaken with the pins.

 

 The Experiment was conducted on pins number PTC7 and PTC6 and abrupt Behavior was absorbed on PTC6.

I am sorry for the error

Regards 

Gopal Rathi. 

 

0 件の賞賛
返信
3,555件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @rathi_tg ,

Unfortunately with the PTC6 and PTC7 is the same situation as above. Both pins are shared on the S32K144EVB with the UART serial connected to the OpenSDA. You can not use them in the same time both for ADC and UART communication, unless if you change the serial. But on this design, the pins are connected to the OpenSDA so this might be the reason why the PTC6 is kept low.

mariuslucianand_0-1604051621297.png

I strongly suggest to have a look on the schematics before starting using the board pins. The schematics and be found here. https://www.nxp.com/webapp/Download?colCode=S32K144EVB-SCH-29248-RB1 

Hope this helps,

Marius

 

 

0 件の賞賛
返信