S32M276 CAN Error when Fee, Mem_43_INFLS, and MemAcc init calls are added

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32M276 CAN Error when Fee, Mem_43_INFLS, and MemAcc init calls are added

311 次查看
Bravin_Link
Contributor II

Here is my Board Initialization setup which allows CAN communication to occur:

Bravin_Link_0-1753302232530.png

Below is where I added the Fee, Mem_43_INFLS, and MemAcc init calls and when I flash to the S32M276 board... CAN no longer works:

Bravin_Link_1-1753302343577.png

Note: I also have a Simulink Initialize Function that has the following for CAN:

Bravin_Link_2-1753302514952.png

 

 

标记 (1)
0 项奖励
回复
0 回复数