S32K14x and MPC57xx toolbox installed at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x and MPC57xx toolbox installed at the same time

Jump to solution
1,681 Views
jakub_bendzala
Contributor II

Hello,

I tried to install two Model-Based Design toolboxes S32K14x and MPC57xx on one PC (one matlab installation) and after installing second toolbox, already installed one completely disappears from matlab and from the file system.

I tried and confirmed this behavior multiple times and on 2 different PCs.

My system specs:

S32K14x toolbox ver. 4.0.0

MPC57xx toolbox ver. 3.0.0

matlab R2018b

win10 x64

Is it possible to have these two toolboxes installed simultaneously?

Is there an workaround available to solve this issue?

Thank you!

Jacob 

0 Kudos
Reply
1 Solution
1,537 Views
mariuslucianand
NXP Employee
NXP Employee

Hello jakub.bendzala‌,

Sorry to hear that!

On DOC-342724 page, if you scroll down to one on my answers, you will find a way to install both toolboxes and use them in the same time.

Best Regards, 

Marius

View solution in original post

2 Replies
1,538 Views
mariuslucianand
NXP Employee
NXP Employee

Hello jakub.bendzala‌,

Sorry to hear that!

On DOC-342724 page, if you scroll down to one on my answers, you will find a way to install both toolboxes and use them in the same time.

Best Regards, 

Marius

1,537 Views
jakub_bendzala
Contributor II

Hi Marius,

Thank you very much!

I searched for relevant answers, but I missed that page, thanks again for your help!

Best,

Jakub

0 Kudos
Reply