S32K144EVB with Simulink has no CAN Output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB with Simulink has no CAN Output

859 Views
WilliamWang0135
Contributor I
  • Windows 10
  • Simulink 2022b
  • MBDT for S32K1xx V4.3.0
  • S32K144EVB-Q100

Problem: We are using S32K144EVB with Simulink MBDT Toolbox. We built a basic CAN communication model based on this video: https://www.nxp.com/pages/introducing-the-can-communication-blocks-from-nxp-mbdt:TIP-INTRODUCING-THE... , but there is no output after we flash the program to the board(tested with an oscilloscope). On the other hand, the board has detectable CAN output when we use it with the example can_pal program on S32DS.

Details:

  • J107 Pin1 and Pin2 connected
  • J16 connected to external 12V supply
  • Tried simple GPIO control on Simulink e.g. lighting up the D11 LED. Used a Constant boolean to control the Digital Write Block, the LED only turned on for a very short period of time after the program is flashed(built and downloaded)
  • Also tried example CAN models provided by the MBDT Toolbox on Simulink but still doesn't work

The related pictures are posted underneath, please feel free to ask me for more information or files, thank you!

Connection StatusConnection StatusCAN Waveform Detectable when Using S32DS can_palCAN Waveform Detectable when Using S32DS can_palCAN Model Built Based on the VideoCAN Model Built Based on the VideoBoard_Config1.pngBoard_Config2.pngBoard_Config3.pngCAN_Config1.pngCAN_Config2.png

0 Kudos
Reply
0 Replies