S32K144: Is there a way to use FlexIO pin for PWM generation in Simulink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144: Is there a way to use FlexIO pin for PWM generation in Simulink

Jump to solution
1,185 Views
mirali
Contributor I

Currently trying to figure out how to use a FlexIO pin for PWM generation in Simulink. I don't see any blocks in Simulink for using a FlexIO pin for PWM generation, only for I2C, SPI and UART. Any help would be greatly appreciated. 

0 Kudos
Reply
1 Solution
1,145 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @mirali ,

Unfortunately, in MBDT for S32K1xx, for the FlexIO we do not provide PWM generation blocks. However, such support can be achieved by using custom code in a similar approach described by this article: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

I am not sure if the S32K1 SDK, the abstraction layer on which the MBDT for S32K1 generates the hardware access peripherals code has such support for the PWM generation, so in this case you can directly control and achieve such functionality by writing to registers using a similar approach mentioned in the article above.

Regards,

Marius

View solution in original post

2 Replies
1,146 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @mirali ,

Unfortunately, in MBDT for S32K1xx, for the FlexIO we do not provide PWM generation blocks. However, such support can be achieved by using custom code in a similar approach described by this article: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

I am not sure if the S32K1 SDK, the abstraction layer on which the MBDT for S32K1 generates the hardware access peripherals code has such support for the PWM generation, so in this case you can directly control and achieve such functionality by writing to registers using a similar approach mentioned in the article above.

Regards,

Marius

1,135 Views
mirali
Contributor I

Thank you for the information

0 Kudos
Reply