S32 Config Tool Prompt Errors at the start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Config Tool Prompt Errors at the start

Jump to solution
1,795 Views
simon98
Contributor IV

Hi

When i launch the S32CT over MBDT for configuring my hardware i noticed that it opens a cmd prompt that it shows this log;

SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.
Sep 24, 2024 6:41:13 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:14 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:14 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:14 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:14 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:14 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:16 PM com.nxp.swtools.common.utils.expression.Expression resolve
SEVERE: [DATA] Error resolving: !(($parent.ARM_Core.getValue() == `ARM_A64_ARCH`) && ($this.getValue() == `true`)), Value of: $parent.ARM_Core not found
Sep 24, 2024 6:41:18 PM com.nxp.swtools.common.utils.expression.Expression resolve
SEVERE: [DATA] Error resolving: !(($parent.ARM_Core.getValue() == `ARM_A64_ARCH`) && ($this.getValue() == `true`)), Value of: $parent.ARM_Core not found
Sep 24, 2024 6:41:18 PM com.nxp.swtools.resourcetables.model.config.ScalarConfig setValue
SEVERE: [DATA] Setting value to a variable/info setting with ID "Gpt.GptChannelConfigSet.GptChannelConfiguration.0.GptChannelTickFrequency"
Sep 24, 2024 6:41:18 PM com.nxp.swtools.resourcetables.model.config.ScalarConfig setValue
SEVERE: [DATA] Setting value to a variable/info setting with ID "Gpt.GptChannelConfigSet.GptChannelConfiguration.1.GptChannelTickFrequency"
Sep 24, 2024 6:41:18 PM com.nxp.swtools.resourcetables.model.config.ScalarConfig setValue
SEVERE: [DATA] Setting value to a variable/info setting with ID "Gpt.GptChannelConfigSet.GptChannelConfiguration.2.GptChannelTickFrequency"
Sep 24, 2024 6:41:18 PM com.nxp.swtools.resourcetables.model.config.ScalarConfig setValue
SEVERE: [DATA] Setting value to a variable/info setting with ID "Gpt.GptChannelConfigSet.GptChannelConfiguration.3.GptChannelTickFrequency"
Sep 24, 2024 6:41:20 PM com.nxp.swtools.resourcetables.model.config.ScalarConfig setValue
SEVERE: [DATA] Setting value to a variable/info setting with ID "Uart.UartGlobalConfig.UartChannel.0.DetailModuleConfiguration.lpuartClockValue"
Sep 24, 2024 6:41:20 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:21 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:21 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:21 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:21 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex
Sep 24, 2024 6:41:21 PM com.nxp.swtools.utils.ConfigurationUtils getEclipseProject
SEVERE: Cannot get container for IPath C:/walvoil/prove/multitasking_led/untitledConfig.mex

 

then the tool opens up.

the configurations of the pin e peripherals works well but i don't lnow if in the future would be the same.

How could i do with this? should i solve it? and if yes, how?

 

Thanks

 

Simon

Tags (4)
0 Kudos
Reply
1 Solution
1,731 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @simon98 

The messages appearing in your log are coming from the eclipse platform on which the S32 Configuration Tools is developed. This seems to be a known issue, already logged in the eclipse community.

However, these messages are not related to a configuration error, and they do not cause any functional problems. As they do not impact the workflow MBDT proposes for configuring the peripherals, pins, and clocks using S32 Configuration Tools, you could simply ignore them.

Please let us know if you encounter any other issues,

Irina

View solution in original post

0 Kudos
Reply
1 Reply
1,732 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @simon98 

The messages appearing in your log are coming from the eclipse platform on which the S32 Configuration Tools is developed. This seems to be a known issue, already logged in the eclipse community.

However, these messages are not related to a configuration error, and they do not cause any functional problems. As they do not impact the workflow MBDT proposes for configuring the peripherals, pins, and clocks using S32 Configuration Tools, you could simply ignore them.

Please let us know if you encounter any other issues,

Irina

0 Kudos
Reply