S12ZVML MINIBRD error 0x80000103

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVML MINIBRD error 0x80000103

1,043 Views
basilmathew
Contributor III

Getting an error while trying to run S12ZVM_FOC_SENSORLESS on MINIBRD . Please find the attached error screen .

Regards,

Basil 

0 Kudos
Reply
2 Replies

836 Views
RadekS
NXP Employee
NXP Employee

Hi Basil,

just idea: The S12ZVML MINIBRD board is hardware design without an external crystal. However, the AN5327 single shunt sensorless software expects external crystal as the clock source. You need to change clock settings from PEE mode to PEI mode when you use AN5327 software.


I hope it helps you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

837 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Basil,

Based on what is see in the screenshot, it appears you do not have a valid connection with the board. 

Please try to toggle the "Stop" button to disconnect and connect back to the target.

Also, the UART baud rate, in the Freemaster settings should be the same as the one set in the Freemaster panel in Simulink.

Hope this helps!

Daniel

0 Kudos
Reply