S-param. Dont work!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S-param. Dont work!

3,684 次查看
vladimirmoscovt
Contributor I

HELP !

Does not work correctly:

MML09212H_400MHz_SP

MML09212H_900MHz_SP

MML09212H_1400MHz_SP

Vladimir. Moscow

uhf.research@mail.ru

标记 (1)
0 项奖励
回复
4 回复数

3,494 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi vladimirmoscovtsev‌,

Can you provide a bit more details? What Matlab Toolbox are you using, what MCU part and what are you trying to do and does not work?

Thank you!

Daniel

0 项奖励
回复

3,494 次查看
vladimirmoscovt
Contributor I

S-param. Dont work!

The issue is not solved.

Check the S-parameters files!!!

0 项奖励
回复

3,494 次查看
constantinrazva
NXP Employee
NXP Employee

Hello vladimirmoscovtsev‌,

Unfortunately, in this community we are only dealing with Matlab/Simulink releated models for NXP/Freescale automotive microprocessors. We do not cover other topics like ultra-high frequency or Advanced Design System (I think that is what you are using in the screenshots provided). Since there is no dedicated community for such topics I would like to suggest you to enter a Support Request here: Support

Hope this helps,

Razvan.

0 项奖励
回复

3,493 次查看
vladimirmoscovt
Contributor I

Hi.

Programm ADS2016.01

>Четверг, 14 июня 2018, 14:21 +03:00 от dumitru-daniel.popa <admin@community.nxp.com>:

>NXP Community

>Re: S-param. Dont work!

>reply from dumitru-daniel.popa in NXP Model-Based Design Tools - View the full discussion

0 项奖励
回复