RBF_File for example uart_world_mpc5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RBF_File for example uart_world_mpc5777C

Jump to solution
2,006 Views
snehalshinde
Contributor I

Hello All,

I am very new to NXP, I am trying to study MBD example uart_hello_world_mpc_5777C example MPC5775B/E-EVB board. Which boatLoader file should I flash from BootLoader -> RBP_Files folder. I tried to flast MPC5777C_S32DS_UART0_CAD0.srec. I do not see any other file with MPC5777C. 

Let me know if I misunderstood anything. 

 

0 Kudos
Reply
1 Solution
1,996 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @snehalshinde ,

That's the file, but you have to do an extra step in the S32DS for the MPC5777C as described below in the Quick Start Guide. You can find the entire document inside the MBDT toolbox installation folder.

mariuslucianand_0-1630568598326.png

Hope this helps,

Marius

 

View solution in original post

0 Kudos
Reply
1 Reply
1,997 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @snehalshinde ,

That's the file, but you have to do an extra step in the S32DS for the MPC5777C as described below in the Quick Start Guide. You can find the entire document inside the MBDT toolbox installation folder.

mariuslucianand_0-1630568598326.png

Hope this helps,

Marius

 

0 Kudos
Reply