RAppID MPC564xL 报错 求助

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RAppID MPC564xL 报错 求助

2,809 次查看
qilie
Contributor I

我在使用Motor Control Development Toolbox for MPC564xL v1.3.0工具包时报错,使用的是MATLAB2013b(正版),错误如图报错.JPG

(Error evaluating 'InitFcn' callback of RAppID_EC_564xL block (mask) 'BSGshell/MicroController Configuration/System_Config/BSGIIV3ISO_Config/RAppID_564xL_Config'.  

Caused by:
Index exceeds matrix dimensions)

之前电脑安装成功,也能正常运行,从新安装系统后,就总是报错,怎么都解决不了,希望得到大家的帮助,谢谢

我的系统是系统.JPG

安装步骤都是按照Motor_Control_Toolbox_Installation_Quick_Start.pdf装的,License也有。

0 项奖励
回复
8 回复数

2,528 次查看
paulvlase
NXP Employee
NXP Employee

Hi ‌,

Can you try the HotFix_2 for MBD Toolbox rev1.3.0 for MPC564xL ?

0 项奖励
回复

2,528 次查看
qilie
Contributor I

Hi Paul Vlase,

        I tried your way, but it didn't work.

(Error evaluating 'InitFcn' callback of RAppID_EC_564xL block (mask) 'BSGshell/MicroController Configuration/System_Config/BSGIIV3ISO_Config/RAppID_564xL_Config'.  

Caused by: Index exceeds matrix dimensions)

I reinstalled the computer system and then came up with this problem. Before that, my MATLAB was working normally. So is it missing in the computer system?

I hope to get your help again。

0 项奖励
回复

2,528 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi ‌,

If you type vol C: in the command line ... 

pastedImage_1.png

Is the Serial Number reported the same with the one from the license file ?

#Account
# License for DISK_SERIAL_NUM=126cb046 dp

Also, that is the extension you are using the license file. Is it *.lic or *.dat ?

Thank you!

Daniel

0 项奖励
回复

2,528 次查看
qilie
Contributor I

Hi  dumitru-daniel.popa

I've done it according to your reply.       But it still doesn't work。qq.JPG

thank you very much!

qilie

0 项奖励
回复

2,528 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi qilie, 

One more thing: can you run this command: lmhostid -vsn 

QQ截图20170619163133.bmp

What is the output on your computer?

Thank you!

Daniel

0 项奖励
回复

2,528 次查看
qilie
Contributor I

Hi  dumitru-daniel.popa

qq2.JPG

Thank you

qilie

0 项奖励
回复

2,528 次查看
Daniel_Popa
NXP Employee
NXP Employee

Ok, so your Disk ID has only 5 valid digits. You need to install this patch: https://community.nxp.com/thread/467975?commentID=1009785#comment-1009785  (HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters) in order to fix the problem. 

Hope this helps!

Daniel

0 项奖励
回复

2,528 次查看
qilie
Contributor I

Hi dumitru-daniel.popa

     I installed this patch, but it doesn't work.

     This problem arises  after the computer reinstalled the operating system. It can be used before reinstalling the operating system. So I think there is something missing from the operating system.

Thank you 

qilie

0 项奖励
回复