Profiler block with referenced models not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Profiler block with referenced models not working

496 Views
Oliver3
Contributor I

Hello,

we are working with the NXP Toolbox and encountered a Problem with the Profiler block, when using it within referenced models: 

If building the referenced model as Top-Model, no error occurs. If building the overall model, during the referenced model build the following error occurs ('missing files'):

Function_Call_Subsystem_private.h:27:29: fatal error: s32k_clock_init.h: No such file or directory #include "s32k_clock_init.h"

Please see also the attachement (example from Profiler with an additional referenced mode).

Is there any workaround or bugfix for this? 

Thank you,

Oliver

0 Kudos
Reply
0 Replies