Not being able to download the generated file directly after the build process in MATLAB Simulink us

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not being able to download the generated file directly after the build process in MATLAB Simulink us

1,151 次查看
Roaa_Baniyounes
Contributor I

I am using:

  • Board: RevC1 EVKB with a MIMXRT1176DVMAA chip.
  • MATLAB Version: 2021a

I did know that the RT1170-EVKB does not support OpenSDA, which means I cannot download the .bin file directly after the build in MATLAB Simulink as described here: "https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Getting-started-with-NXP-i-MX-RT1xxx-Simul...".

There are two other download types (see attached picture) but it did not work. I attempted to use the MCU-Link download option and specified the necessary paths, but the process only generated the binary file without downloading it to the board.

How can I configure the download options in Simulink's hardware settings to ensure the generated binary file is successfully downloaded to the RT1170-EVKB board after the build process?

标记 (1)
0 项奖励
回复
0 回复数